Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum 2N7000 as VCR
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 6 answers
  • Subscribers 308 subscribers
  • Views 4188 views
  • Users 0 members are here
  • mosfets
  • attiny85
  • voltage controlled resistor
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

2N7000 as VCR

tibmeister
tibmeister over 9 years ago

Ok, so going to start off by stating the issue I am facing, Q1 (2N7000) is getting hot enough to cook with.  Seriously, I'm measuring 50C on the sucker.  What I can't figure out is why.  Now I will state, I am far from an engineer, I am easily classified as a noob.

 

Anyway, I have attached my schematic.  The sensor has a resistive heater that is driven by Q1 on the HA pin, and the trick is it has to cycle between +5VDC and +1.4VDC at regular intervals.  So since I am using an ATTiny85 (I love these little guys!) I'm looking at max Vout on the IO pin of +4.85VDC @ ~20mA.  So, I came up with using the LM324 as a small amp to bring my IO up to a full +5VDC and then as a buffer to ensure that even as I put load on Q1 Source I will maintain the desired voltage at the sensor's HA pin.  This may not be the best way to do this, but like I said, noob here.

 

So, if my calculations are correct, G1 of the LM324 should represent about a 10% amplification of Vin.  So at most I'm pushing something in the neighborhood of +5.5VDC into V+ of the LM324 G2, which should be well within specs.  As far as Q1, since I'm using it as a voltage controlled resistor I'm not running Q1 into saturation, which I don't think is bad but I'm almost wondering if my heat issue is coming from the fact that on the drain of Q1 I have +12V and on the source I have +1.4-5VDC, so that's a lot of Vdrop which I'm sure turns into wattage and dissipated heat.

 

I am struggling with this one and hoping someone could get my head straight on it.  Oh and yes, I have a lot of filtering caps and zener diodes for over-voltage protection.  It's cheap insurance in my mind having the zeners, and the caps, well it can't hurt to filter out any in-rush current image.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 9 years ago +1 suggested
    Using a power fet as a heater is not that great of an idea in practice as a warm fet has lowered Zin with low gain Switching resistors is a better idea as they are made to be heaters a bipolar Q cheap…
  • tibmeister
    tibmeister over 9 years ago in reply to Robert Peter Oakes +1
    Are you kidding, I've actually begun to understand this stuff much more than I thought I would and that alone is priceless. As for the offset, Rds(on) is 5.3 ohm and the current drain from source to drain…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    The FET is going to follow the OPAMP output -~4V with a threshold of about 2V (the V difference between gate and source where it starts to turn on)

     

    If the FET was to be turned fully on then you have a resistor divider between the 220 and 33 resistor so the max that will be output is about 1.5V as the resistance of the FET is negligable so you will never get the full 5V no matter what you do, perhaps switching around the 33 and 220

     

    what is the resistance of the heater ??

     

    with regard to the buffer opamp, it will try to get its - input the same as the + so if you have 5V on the +, the output should try to go to about 7-9V depending on the load (AKA the 33ohm + Heater), the 220ohm will severely limit the current flow which is why it wont ever get to the desired voltage and the opamp will or should be going to the + rail (12V)

     

    if the fet is hard on then your current will be about 50mA without the heater connected but even if it is connected it will never exceed 68mA due to the 220 Ohm  (Remember I=V/R)

     

    If you tell me / the community what the heater needs then I can tell you what resistor values you need

     

    Last question, how are you planning on getting the 5V and 1.5V outputs, the current design will only give one volt setting. not two

     

    Ok, regarding the heat, 50mA at 12V is 576mW which if this was across the FET it would be at its limit but in the schematic you show, all the volts will be dropped across the 220ohm resistor so it will be or should be getting hot, not the FET.

     

    like I said, swap the 220 and 33 ohm resistors, it should work much better (This is without knowing your real load parameters), with this design you could also remove the 220 altogether and connect the top of the fet directly to 12V, I would still put a 220 or more instead of the 33 Ohm though.

     

    Hope this helps for now, provide the feedback and I can help more

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    The FET is going to follow the OPAMP output -~4V with a threshold of about 2V (the V difference between gate and source where it starts to turn on)

     

    If the FET was to be turned fully on then you have a resistor divider between the 220 and 33 resistor so the max that will be output is about 1.5V as the resistance of the FET is negligable so you will never get the full 5V no matter what you do, perhaps switching around the 33 and 220

     

    what is the resistance of the heater ??

     

    with regard to the buffer opamp, it will try to get its - input the same as the + so if you have 5V on the +, the output should try to go to about 7-9V depending on the load (AKA the 33ohm + Heater), the 220ohm will severely limit the current flow which is why it wont ever get to the desired voltage and the opamp will or should be going to the + rail (12V)

     

    if the fet is hard on then your current will be about 50mA without the heater connected but even if it is connected it will never exceed 68mA due to the 220 Ohm  (Remember I=V/R)

     

    If you tell me / the community what the heater needs then I can tell you what resistor values you need

     

    Last question, how are you planning on getting the 5V and 1.5V outputs, the current design will only give one volt setting. not two

     

    Ok, regarding the heat, 50mA at 12V is 576mW which if this was across the FET it would be at its limit but in the schematic you show, all the volts will be dropped across the 220ohm resistor so it will be or should be getting hot, not the FET.

     

    like I said, swap the 220 and 33 ohm resistors, it should work much better (This is without knowing your real load parameters), with this design you could also remove the 220 altogether and connect the top of the fet directly to 12V, I would still put a 220 or more instead of the 33 Ohm though.

     

    Hope this helps for now, provide the feedback and I can help more

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer