Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Choosing the correct multiconductor wire size
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 339 subscribers
  • Views 1363 views
  • Users 0 members are here
  • frontpage
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Choosing the correct multiconductor wire size

e14 Contributor
e14 Contributor over 10 years ago

I have multiple solenoid valves I want to supply control power via a multi conductor cable. Each valve draws .8 amps at 120v. I could use 22awg size wire in my cable for the wires operating each valve. My question is about the common wire. Since that wire is common to all the valves will I have to size my wire based on the current running through that wire? Am I correct in thinking that if all four solenoids were active at once then the common wire would be carrying a load of ~4 amps? (4 sol x .8 amps each) so the common wire would need to be sized at 18awg? This sounds like such a novice question I know. Any help would be appreciated!

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    As far as your basic question, you are correct

     

    4 relays consuming just under an amp each with a common return will result in 4 Amps flowing in the return wire when all are on so it must be sized to handle that load. what also needs consideration is the distance between the control point and the relay, if too far then you may need bigger gauge wire to compensate for losses in the wire

     

    You need to ensure you have protection across the load as well to protect back emf from blowing the control circuits, these may already be in the relays or the controller but make sure they exist, if not then add them (This is sometimes called a snubber network). If the Solenoids are DC then a Diode across the solenoid will work but I assume you're using AC due to being a common mains voltage, and in this case the snubber will be across the switch

    Image result for solenoid snubber network

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    As far as your basic question, you are correct

     

    4 relays consuming just under an amp each with a common return will result in 4 Amps flowing in the return wire when all are on so it must be sized to handle that load. what also needs consideration is the distance between the control point and the relay, if too far then you may need bigger gauge wire to compensate for losses in the wire

     

    You need to ensure you have protection across the load as well to protect back emf from blowing the control circuits, these may already be in the relays or the controller but make sure they exist, if not then add them (This is sometimes called a snubber network). If the Solenoids are DC then a Diode across the solenoid will work but I assume you're using AC due to being a common mains voltage, and in this case the snubber will be across the switch

    Image result for solenoid snubber network

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    Thanks for the reply! The protection is built into the output cars of the allen bradley I/O rack.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer