Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Which one is the culprit: Mobo or Power Supply?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 313 subscribers
  • Views 967 views
  • Users 0 members are here
  • troubleshooting
  • ac-dc converter
  • ac-dc_power_bricks
  • power-supply
  • Motherboard
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Which one is the culprit: Mobo or Power Supply?

Former Member
Former Member over 9 years ago

Seriously, I need to find out.  Usually, I have sufficient motherboards and power supplies to try swapping out one for the other (did the problem move or cease to exist?).  Unfortunately, I am down to my last odd motherboard and last odd power supply.  The good news, of course, is that the better half is happy that my "techie junk" has diminished substantially!  But, I digress.

 

Mobo: Biostar NM70I-1037U Mini-ITX with Dual-core Celeron 1037U processor

Worked successfully 1 year ago with another power supply and then it and the RAM was put safely away (sealed in plastic).

 

Power Supply: Mini-Box picoPSU-160-XT High Power 24 Pin for Mini-ITX (small-ish)

Worked successfully 6 months ago with a different mobo and then it was put safely away (sealed in plastic).

 

Today, I completed a build with the mobo, power supply,  a Thermaltake Cube V1 enclosure (includes a case fan), RAM (previously sealed sway), CPU fan (supposedly not needed according to Biostar but I am paranoid), and an SSD.  I attempted to power up with 2 different AC/DC power adapters:

  1. 12V, 5A
  2. 19V, 2.1A.

 

1. Observed symptoms with a 12V 5A AC/DC adapter

Push power button.

    Loop forever         Both fans and power indicator light on for 1 second         Both fans and power indicator light off for 2-3 seconds     End of loop

2. Observed symptoms with a 19V 2.1A AC/DC adapter

Push power button.

Power light comes on and stays on forever.

Fans do not activate.

 

Is it the mobo or the power supply?

Opinions, please.

 

Also, suggestions for further testing, aside from sticking the suspect power supply in another build which I don't have at the moment?

 

Thank you in advance.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    Looking at picoPSU-160-XT, 160watt (200watt peak) , 12V input DC-DC ATX Power Supply , they suggest a 12V 12.5 A AC-DC switching supply. The other thing a noticed is a 4 square plug for power on the Biostar board. Did you plug into that?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    clem57 Thanks, that was my miss.  I will try one today or tomorrow (time permitting) at my local Altex Computer store (near Frankford @ Midway in Carrolton TX USA).  That store is very helpful/flexible.  Yes, the 4 square plug is inserted correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    clem57 Thanks, that was my miss.  I will try one today or tomorrow (time permitting) at my local Altex Computer store (near Frankford @ Midway in Carrolton TX USA).  That store is very helpful/flexible.  Yes, the 4 square plug is inserted correctly.