Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Transistor question
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 305 subscribers
  • Views 722 views
  • Users 0 members are here
  • frontpage
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Transistor question

Former Member
Former Member over 9 years ago

I have a project that I am working on that requires me to be able to control the state of a Coax or BNC Connector connected between a satellite receiver and LNB(Dish). The cable is rated at 75ohm, carries 18v DC and a freq of up to 3GHz. This circuit is not to split a satellite signal but to simply connect/disconnect the receiver/line from the LNB with little to no loss in voltage or signal.

 

I am using a ATmega328P to 74HC595 8-Bit Shift Register to control multiple connectors. However, I am unsure which transistor, if any, will support the cable ratings I need with little to no loss if possible.

 

If that is not possible, would anybody have any ideas how else I could control the connectors?

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • pettitda
    pettitda over 9 years ago +1
    For low loss, you need a RF switch (75ohm) as opposed to a transistor. There are many available on the market which will work up to 3 GHz (Try Macom, Skyworks, Perregrine Semi, etc). However, it is likely…
  • michaelkellett
    michaelkellett over 9 years ago +1
    You could use relays - look for a second hand co-axial part if you only want one or you could make a pcb (tricky layout issues!!!) and use things like this from Digikey 374-1041-1-ND. MK
Parents
  • Former Member
    0 Former Member over 9 years ago

    I can look into pin diodes to see if that will work for me and so far it sounds like it will.

     

    Thanks for the help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago

    I can look into pin diodes to see if that will work for me and so far it sounds like it will.

     

    Thanks for the help.