Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Real problems with cabling for a Beaglebone-Black-Wireless
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 313 subscribers
  • Views 480 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Real problems with cabling for a Beaglebone-Black-Wireless

raife
raife over 8 years ago

Hi,

     I just got a Beaglebone-Black-Wireless kit. I have powered-up the Beaglebone via a Linux-laptop and it works. However, I would like to connect the Beaglebone to a monitor and USB keyboard and mouse (as stated in the included instructions for setting-up the computer). The problem is that, after trying every cable and adapter I have access to, I simply cannot plug in any USB-cable into the Beaglebone at the same time that any micro-HDMI plug is plugged-in. The two, simply will not fit at the same time. The physical connectors (for the full-sized USB Host-port, and the micro-HDMI on the Beaglebone circuit-board) are on opposite sides, of the same edge of the circuit-board, and are just too close together for every pair of cables I can find. The connectors overlap each other enough to prevent both being plugged-in, at the same time. The only help I have gotten elsewhere is the suggestion to physically cut-down the cable-ends to try to make them fit. This can't be right.  I know that many people are running this computer, and most of the instructions for using it, simply assume that the computer is hooked-up as a GUI-based, Linux computer, controlled with a mouse and keyboard. So, why can't I connect these devices? Or, where can I get USB, and micro-HDMI, cables that can both be plugged into the Beaglebone at the same time?

  • Sign in to reply
  • Cancel

Top Replies

  • raife
    raife over 8 years ago +1
    UPDATE: I ordered two different HDMI-cables from Amazon... the "amazonbasics" six-foot (micro-to-full-size) cable, and the "Rankie" six-foot (micro-to-full-size) cable. Both fit in the tight-space on the…
Parents
  • raife
    0 raife over 8 years ago

    UPDATE: I ordered two different HDMI-cables from Amazon... the "amazonbasics" six-foot (micro-to-full-size) cable, and the "Rankie" six-foot (micro-to-full-size) cable. Both fit in the tight-space on the BBB, and work. The molded-plastic cable-ends are a little tight, against each other, but it does not prevent the HDMI-cables from being plugged-in at the same time as a full-sized USB cable. So, I can now use the "Beaglebone-Black-Wireless" board. It seems my other micro-HDMI cable-ends were just a little larger compared to these HDMI-cables.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • raife
    0 raife over 8 years ago

    UPDATE: I ordered two different HDMI-cables from Amazon... the "amazonbasics" six-foot (micro-to-full-size) cable, and the "Rankie" six-foot (micro-to-full-size) cable. Both fit in the tight-space on the BBB, and work. The molded-plastic cable-ends are a little tight, against each other, but it does not prevent the HDMI-cables from being plugged-in at the same time as a full-sized USB cable. So, I can now use the "Beaglebone-Black-Wireless" board. It seems my other micro-HDMI cable-ends were just a little larger compared to these HDMI-cables.