Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Electronic know how
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 8 answers
  • Subscribers 336 subscribers
  • Views 2096 views
  • Users 0 members are here
  • repairing
  • no schematics
  • learning
  • electronics
  • bad grammar
  • knuckle dragger
  • 3rd eye
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Electronic know how

malus_lupus
malus_lupus over 8 years ago

When it comes to repairing electronics I to an extent have it under control. However, I can't do as many people do and look at a board and know what it is used for I just find the broken component and fix it. It is all good and such til you need to know how to fix a board that seems perfectly fine or resolder wires that became disconnected. I work in an area where there are no schematics for what I do. I recently had to learn transistors npn and pnp to get a clue (still am unsure about the blue wire).

I still have no clue what the board does and that is one thing I would like to be able to figure out by looking at the board. I see people do it all the time they see the power goes in, goes through x components (I know the name of most) thus it equals this type of board thus if it seems to be doing this it should be x reason check-in x area. I just look and see if there are messed up components etc and hope that is the answer which isn't the case always.

I have an X-box plug that I have no clue what went wrong (cheap ones). It has 120 volts coming in but not 12v coming out all parts look brand new the solder joints are crappy but no cracks. I have no clue what is wrong because I do not know the story entire of the board. I know it comes in 120v ac goes through a component eventually hits a transformer turns into the 12v and I dunno why the rest of the components exists. I know some smooth it out. I dunno what splits it into a 12v and 5v. I do not know a good way to test it without 120v coursing through it which I honestly do not want to do.

I have a weird gap in my electronic know how is there a video series on how a board tells a story per se instead of just look for this to repair it. Sometimes I need to be able to figure out what a board does so I can fix it be it wires popped off, or an X box power supply. Neither have schematics and the x box power supply boards change from each one because of pricing. One was smothered in roaches so that one is probably obvious and the other was clean. Albeit after cleaning the roaches out the parts looked brand new, no bulging caps, no burnt resistors, the joints were shoddy but they were not cracked.

Ben does a decent job of showing a talent like this he may do research I am unsure but I have seen others (bigclivedotcom) pick up a board and instantly knows that goes to x and go hmm... that circuitry is for w and this is for y but this one is an oddity on z it is probably used for A, and they just took it off something random without usually looking at the schematics. I do not even know why the companies choose some components they do instead of others that would do as good as a job or seem like they would.

I am going to try and give you a pic of a board (bad quality but my phones camera is not the best) and you will see immediately what goes to what and how the board works and why it works how it works. I see a board that has parts I know how the parts work partially and I know where some wires need to be resolder back on and the rest of the wires will need to be probed to even figure out what they do and where to put them if I figure it out. I wish to have your eyes and brains to be able to instantly know this stuff. I know I have been redundant but I also I know I am not the best at explaining myself so I end up explaining myself twice in different ways hoping I convey the message.

*Sidenote if it helps: This board goes to a Halloween decoration it makes sound and has two LEDs for eyes. The switch I believe is a double pole double throw you flip it one way it makes sound and lights up, you flip it another it just lights up. I personally almost feel the board is unnecessary if not for that chip hiding under the black resin. Which is most likely where the sounds are housed. I wish to repair it to firstly save money and secondly learn. That's about it. Thanks for any help.





Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +6 suggested
    Hi Justin, What you're doing to seek to repair is no different to what most engineers do, i.e. just visually observe if anything looks out of place or burnt up. Most consumer electronics has no circuit…
  • jw0752
    jw0752 over 8 years ago +6 suggested
    Hi Justin, I have to disagree slightly with shabaz . The Art of Electronics is a very good book but for the Electronics Repair person I would choose this book as it is more practical and more down to earth…
  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Justin, It sounds like you are well on your way to understanding what is going on. You certainly have the first ingredient, which is a healthy curiousity. Time and experience will help you as you continue…
Parents
  • mcb1
    0 mcb1 over 8 years ago

    Like jw0752 and shabaz indicated, you are well on the way.

     

    For some of us it's been 30+ years of experience to reach this point and we've been exposed to lots of these situations.

    It doesn't always translate that years = experience and I work with some very knowledgeable people that I would suggest are at your level when it comes to fixing broken boards.

     

    I've fixed countless boards with no schematics, and the clue is being able to recognise what is broken/damaged or what it does/doesn't do.

    At some point you do need to be able to check that your repair has been effective.

     

    Every board needs power, and often it is the first problem. Later boards that use High frequency DC/DC converters (like your X-Box) have capacitors that have limited life and these wear and become ineffective, which causes issues. They tend to bulge or even leak.

     

    Identifying outputs that control the LED's (as in your example) means you can test that these are working without having to understand the inner workngs or programming of the micro-controller.

     

    Finally one skill you'll need is the abilty to produce a schematic from the physical items.

    It usually involves a couple of redraws as you tidy up your findings and work out the full interaction of the interconnections.

    Input on the left, output on the right, positive power at the top with ground at the bottom will help later when using it.

    Often you might only need a few parts to enable a repair.

     

    This skill gets better with practice and attention to detail, and identifying the parts requires access to datasheets or information about the components.

    Boards such as your LED with the COB (Chip on board) hide the controller and these can't be identified, so you're left to prove the outputs, LEDs and switch.

     

     

    I'm sure I could identify a number of boards by looking at them, and there are clues that you'll soon pickup.

    Most boards have a number or description that you can use in search engines. Some LCD monitors use generic manufacturers boards and simply add their logo on the front face, and these popup in forums, or spares suppliers.

     

     

    Cheers

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago

    Like jw0752 and shabaz indicated, you are well on the way.

     

    For some of us it's been 30+ years of experience to reach this point and we've been exposed to lots of these situations.

    It doesn't always translate that years = experience and I work with some very knowledgeable people that I would suggest are at your level when it comes to fixing broken boards.

     

    I've fixed countless boards with no schematics, and the clue is being able to recognise what is broken/damaged or what it does/doesn't do.

    At some point you do need to be able to check that your repair has been effective.

     

    Every board needs power, and often it is the first problem. Later boards that use High frequency DC/DC converters (like your X-Box) have capacitors that have limited life and these wear and become ineffective, which causes issues. They tend to bulge or even leak.

     

    Identifying outputs that control the LED's (as in your example) means you can test that these are working without having to understand the inner workngs or programming of the micro-controller.

     

    Finally one skill you'll need is the abilty to produce a schematic from the physical items.

    It usually involves a couple of redraws as you tidy up your findings and work out the full interaction of the interconnections.

    Input on the left, output on the right, positive power at the top with ground at the bottom will help later when using it.

    Often you might only need a few parts to enable a repair.

     

    This skill gets better with practice and attention to detail, and identifying the parts requires access to datasheets or information about the components.

    Boards such as your LED with the COB (Chip on board) hide the controller and these can't be identified, so you're left to prove the outputs, LEDs and switch.

     

     

    I'm sure I could identify a number of boards by looking at them, and there are clues that you'll soon pickup.

    Most boards have a number or description that you can use in search engines. Some LCD monitors use generic manufacturers boards and simply add their logo on the front face, and these popup in forums, or spares suppliers.

     

     

    Cheers

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
No Data