Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Electronic know how
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 8 answers
  • Subscribers 336 subscribers
  • Views 2104 views
  • Users 0 members are here
  • repairing
  • no schematics
  • learning
  • electronics
  • bad grammar
  • knuckle dragger
  • 3rd eye
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Electronic know how

malus_lupus
malus_lupus over 8 years ago

When it comes to repairing electronics I to an extent have it under control. However, I can't do as many people do and look at a board and know what it is used for I just find the broken component and fix it. It is all good and such til you need to know how to fix a board that seems perfectly fine or resolder wires that became disconnected. I work in an area where there are no schematics for what I do. I recently had to learn transistors npn and pnp to get a clue (still am unsure about the blue wire).

I still have no clue what the board does and that is one thing I would like to be able to figure out by looking at the board. I see people do it all the time they see the power goes in, goes through x components (I know the name of most) thus it equals this type of board thus if it seems to be doing this it should be x reason check-in x area. I just look and see if there are messed up components etc and hope that is the answer which isn't the case always.

I have an X-box plug that I have no clue what went wrong (cheap ones). It has 120 volts coming in but not 12v coming out all parts look brand new the solder joints are crappy but no cracks. I have no clue what is wrong because I do not know the story entire of the board. I know it comes in 120v ac goes through a component eventually hits a transformer turns into the 12v and I dunno why the rest of the components exists. I know some smooth it out. I dunno what splits it into a 12v and 5v. I do not know a good way to test it without 120v coursing through it which I honestly do not want to do.

I have a weird gap in my electronic know how is there a video series on how a board tells a story per se instead of just look for this to repair it. Sometimes I need to be able to figure out what a board does so I can fix it be it wires popped off, or an X box power supply. Neither have schematics and the x box power supply boards change from each one because of pricing. One was smothered in roaches so that one is probably obvious and the other was clean. Albeit after cleaning the roaches out the parts looked brand new, no bulging caps, no burnt resistors, the joints were shoddy but they were not cracked.

Ben does a decent job of showing a talent like this he may do research I am unsure but I have seen others (bigclivedotcom) pick up a board and instantly knows that goes to x and go hmm... that circuitry is for w and this is for y but this one is an oddity on z it is probably used for A, and they just took it off something random without usually looking at the schematics. I do not even know why the companies choose some components they do instead of others that would do as good as a job or seem like they would.

I am going to try and give you a pic of a board (bad quality but my phones camera is not the best) and you will see immediately what goes to what and how the board works and why it works how it works. I see a board that has parts I know how the parts work partially and I know where some wires need to be resolder back on and the rest of the wires will need to be probed to even figure out what they do and where to put them if I figure it out. I wish to have your eyes and brains to be able to instantly know this stuff. I know I have been redundant but I also I know I am not the best at explaining myself so I end up explaining myself twice in different ways hoping I convey the message.

*Sidenote if it helps: This board goes to a Halloween decoration it makes sound and has two LEDs for eyes. The switch I believe is a double pole double throw you flip it one way it makes sound and lights up, you flip it another it just lights up. I personally almost feel the board is unnecessary if not for that chip hiding under the black resin. Which is most likely where the sounds are housed. I wish to repair it to firstly save money and secondly learn. That's about it. Thanks for any help.





Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +6 suggested
    Hi Justin, What you're doing to seek to repair is no different to what most engineers do, i.e. just visually observe if anything looks out of place or burnt up. Most consumer electronics has no circuit…
  • jw0752
    jw0752 over 8 years ago +6 suggested
    Hi Justin, I have to disagree slightly with shabaz . The Art of Electronics is a very good book but for the Electronics Repair person I would choose this book as it is more practical and more down to earth…
  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Justin, It sounds like you are well on your way to understanding what is going on. You certainly have the first ingredient, which is a healthy curiousity. Time and experience will help you as you continue…
Parents
  • malus_lupus
    0 malus_lupus over 8 years ago

    Thanks for the advice. With this Halloween thing I realized I do not need to have the LEDs rigged how they are, and I found a motor that was not connected I know how to rig them to work somewhat proper the motor should pop up and down which means it should have a contact point that has a fluctuation between positive x and negative x but I have yet to find one I found one that goes from 0 to .x that seems more LED blinking lights than anything. I can rig the motor up with a double throw double pole reverse polarity switch if need be (it would be manual but I can deal with that). However, the audio oy vey I want that to work. I have it connected up according to what the board says speaker to speaker proper negative and positive but it refuses to work I even short the switch that goes to it to make sure it is always on while testing but nothing. Even if I jotted down the board in a schematic way I would not know exactly what to do for me to make the audio work. I have also discovered a very very odd thing on this that I have no clue what it does. It does not put out voltage, it is not connected to ground I do not think, however it does have 2 wires that come out of it and connect to a transistor.

    Here are some pics of the board. With some identity marks. I found where the blue wires go they are the speaker both are blue positive and negative it goes in the blue circle. The yellow circle is where the yellow wire goes from another switch presumably positive I have no clue where the negative for that switch goes it was disconnected when I got into it. I wired the board back together according to the pics I got of it before a lot of wires popped off bad soldering job cheap board etc. I however no longer need the eyes to flicker and there is no motor connection on the board as far as I can tell. Also the mysterious circle with green wires. I also will include a switch image so you can see how it was wired when I got it.

    (the speaker works I tested and found out once by accident way back at the beginning before the wires started popping off. Scared me because I had no clue it had speakers.Yes, a pad popped off sadly dunno when or how but it is a cheap board and the connection still works. It gets power all over the board minus the mysterious green area.)
    The


    imageimageimageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • malus_lupus
    0 malus_lupus over 8 years ago

    Thanks for the advice. With this Halloween thing I realized I do not need to have the LEDs rigged how they are, and I found a motor that was not connected I know how to rig them to work somewhat proper the motor should pop up and down which means it should have a contact point that has a fluctuation between positive x and negative x but I have yet to find one I found one that goes from 0 to .x that seems more LED blinking lights than anything. I can rig the motor up with a double throw double pole reverse polarity switch if need be (it would be manual but I can deal with that). However, the audio oy vey I want that to work. I have it connected up according to what the board says speaker to speaker proper negative and positive but it refuses to work I even short the switch that goes to it to make sure it is always on while testing but nothing. Even if I jotted down the board in a schematic way I would not know exactly what to do for me to make the audio work. I have also discovered a very very odd thing on this that I have no clue what it does. It does not put out voltage, it is not connected to ground I do not think, however it does have 2 wires that come out of it and connect to a transistor.

    Here are some pics of the board. With some identity marks. I found where the blue wires go they are the speaker both are blue positive and negative it goes in the blue circle. The yellow circle is where the yellow wire goes from another switch presumably positive I have no clue where the negative for that switch goes it was disconnected when I got into it. I wired the board back together according to the pics I got of it before a lot of wires popped off bad soldering job cheap board etc. I however no longer need the eyes to flicker and there is no motor connection on the board as far as I can tell. Also the mysterious circle with green wires. I also will include a switch image so you can see how it was wired when I got it.

    (the speaker works I tested and found out once by accident way back at the beginning before the wires started popping off. Scared me because I had no clue it had speakers.Yes, a pad popped off sadly dunno when or how but it is a cheap board and the connection still works. It gets power all over the board minus the mysterious green area.)
    The


    imageimageimageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
No Data