Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Measuring capacitors in circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 10 answers
  • Subscribers 341 subscribers
  • Views 16024 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Measuring capacitors in circuit

Andy Betts
Andy Betts over 8 years ago

Simple question really...... Is there an accurate way of measuring the capacitance of a non polarised capacitor whilst it's still in circuit??

 

I don't have a scope, but I do have a DMM and an ESR that tests resistors, transistors and capacitors.

 

Thanks in advance

 

Andy

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago in reply to Andy Betts +3 suggested
    Hi Andy, I used to cut traces and wires temporarily in order to isolate the part in question. It is only necessary to break the circuit on one side. After the test one just patches the break and moves…
  • snidhi
    snidhi over 8 years ago in reply to Andy Betts +3 suggested
    Another way would be to remove it physically from the circuit (if possible) and then measure it and solder back a new one
  • balearicdynamics
    balearicdynamics over 8 years ago +3
    Thank you for this goo question I have read great explanation and good answers. Enrico
Parents
  • genebren
    0 genebren over 8 years ago

    Andy,

     

    There are some techniques that can be used to minimize the effects of parallel paths around components that you are trying to measure.  I spent 10 years of my career working on in-circuit or 'bed of nails' testers that  were used to measure each component on a board to validate value, function and/or operation.  We used a method of guarding to break parallel paths, effecting the component that we were attempting to measure.  Depending on the device that you are using to measure the component, you might be able to perform a similar test.  The concept is base on the measurement device having stimulus on one lead (for capacitors this might be either an A/C or D/C signal) and the measurement is performed on the other lead.  Guarding would attempt to inject the same stimulus signal into the parallel path to prevent current flow (same potential on either side of the parallel path meant no current would flow).  Guarding will not always work.  It has difficulty with low impedance paths and also some active paths.

     

    From your schematic, it was not clear which component(s) you were attempting to measure.  Can you provide any additional information?

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • genebren
    0 genebren over 8 years ago

    Andy,

     

    There are some techniques that can be used to minimize the effects of parallel paths around components that you are trying to measure.  I spent 10 years of my career working on in-circuit or 'bed of nails' testers that  were used to measure each component on a board to validate value, function and/or operation.  We used a method of guarding to break parallel paths, effecting the component that we were attempting to measure.  Depending on the device that you are using to measure the component, you might be able to perform a similar test.  The concept is base on the measurement device having stimulus on one lead (for capacitors this might be either an A/C or D/C signal) and the measurement is performed on the other lead.  Guarding would attempt to inject the same stimulus signal into the parallel path to prevent current flow (same potential on either side of the parallel path meant no current would flow).  Guarding will not always work.  It has difficulty with low impedance paths and also some active paths.

     

    From your schematic, it was not clear which component(s) you were attempting to measure.  Can you provide any additional information?

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer