Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Measure the volume change of a battery cell
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 5 answers
  • Subscribers 316 subscribers
  • Views 1318 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Measure the volume change of a battery cell

zeyang
zeyang over 7 years ago

Hello,

 

I would like measure the volume change of a lithium ion pouch cell during charge and discharge. The volume change will mainly reflect on the thickness of the battery. When it is discharged it is about 7 mm and it will increase by about 10% when it is charged. I would like to track the changes during charging.

 

We find this component as below which is a linear motion potentiaometer. https://se.farnell.com/ab-elektronik/4114902470/sensor-linear-5-kohm-20-flange/dp/2311430

  • ±20% Selection tolerance
  • ± 2.0% Typical independent linearity
  • 10mm ± 0.5mm Effective travel

 

Does the 20% means the accuracy of the potentiometer?

 

Do you have any suggestions about other type of sensors that I could use for this kind of measurement?

 

Thanks a lot for the help!

 

Best Regards,

 

/Zeyang

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +4 suggested
    You could also try capacitance measurement. If you put a foil "plate" on the battery and measure the capacitance to a nearby metal plate, the distance between plates will be directly proportional to the…
  • michaelkellett
    michaelkellett over 7 years ago +4 suggested
    You could do the measuring with Mitutoyo 575123 (Farnell 1667327 £169) - it outputs data in Mitotyo format so you need an interface and neither Farnell nor RS seem to sell these ! You can buy the interface…
  • shabaz
    shabaz over 7 years ago +3 verified
    Hi Zeyang, I think you're right, it is likely the overall resistance tolerance. But I think the 750 gram needed to operate this sensor could be too high for your application maybe? I don't know how much…
Parents
  • michaelkellett
    0 michaelkellett over 7 years ago

    You could do the measuring with Mitutoyo 575123 (Farnell 1667327 £169)  - it outputs data in Mitotyo format so you need an interface and neither Farnell nor RS seem to sell these !

     

    You can buy the interface from:

     

    https://gb-greatgages.glopalstore.com/search?type=product&q=Mitutoyo+USB+Data+Input+Tool

     

    And they also sell a range of other displacement gauges and interfaces, as Shabaz suggested pick low force one - I seem to remember that you can remove the springs from some of the Mititoyo ones.

     

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 7 years ago

    You could do the measuring with Mitutoyo 575123 (Farnell 1667327 £169)  - it outputs data in Mitotyo format so you need an interface and neither Farnell nor RS seem to sell these !

     

    You can buy the interface from:

     

    https://gb-greatgages.glopalstore.com/search?type=product&q=Mitutoyo+USB+Data+Input+Tool

     

    And they also sell a range of other displacement gauges and interfaces, as Shabaz suggested pick low force one - I seem to remember that you can remove the springs from some of the Mititoyo ones.

     

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer