Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Repair Challenge: XBOX ONE S! (Beep on then beep off)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 57 replies
  • Answers 7 answers
  • Subscribers 352 subscribers
  • Views 47385 views
  • Users 0 members are here
  • xbox
  • helpme
  • repair
  • xbox one s
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Repair Challenge: XBOX ONE S! (Beep on then beep off)

lilithelotor
lilithelotor over 8 years ago

CLARIFICATION

YES, BEFORE STARTING WORK ON THIS OF COURSE I GOOGLED AND WATCHED SEVERAL VIDEOS (MOSTLY USELESS) AND READ RESOURCES ON COMMON XBOX ONE AND ONE S PROBLEMS.

 

  1. I tried the HDD in a PC, and it does show up as several NTFS partitions with files that all look fine.
  2. Blu Ray drive at least powers up and can insert and eject a disc.
  3. Tried the "cold mode hairdrier" trick to spin the fan manually. It's not the fan. The fan works.

All other components of the board seem to work. Just the system started up with a startup sound, and shut down with a shut down sound immediately after. Likely a protection being triggered.

 

Help meee!

 

Trying to figure out this XBOX One S issue: https://www.ifixit.com/Answers/View/523582/PSU+11... Any ideas?

 

It makes the start and then stop sound. Southbridge gets voltage. All 12V test points get voltage. Power rails to CPU suspiciously low resistance. Details in iFixit link.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


I have an XBOX ONE S that I bought as “for parts” on eBay and the owner says it was kept in a clean house, etc. It is indeed clean inside. No signs of water damage.

The PSU is also fine. The APU had a TON of thermal grease all over the surface mount capacitors. I didn’t remove that yet but I did re-apply some arctic silver and I used a more reasonable amount.

The symptoms I see:

Console when plugged in does a few quick pulses to the APU fan. Is it trying to init?

Console when eject is pressed makes the eject sound, then the shutdown sound immediately after.

Console when power is pressed makes startup beep and then shutdown beep immediately after.

I don’t know what kind of issue I’m getting yet. Is there a JTAG interface or some way to do further diagnosis on this thing?

11.94V sounds perfectly fine for a 12V rail. Should I simpy try plugging a PC power supply into the motherboard to see if it will boot?

Any links or info on diagnosis would be appreciated.

Thanks in advance!


later

Aha! In the image you can see the CPU filter capacitor is registering just 1 ohm! The others are pretty low too but I bet if I remove that one it’ll at least boot. I have a server motherboard with a broken socket that I can steal capacitors from. Might replace the whole row if necessary.

image


later still

Looks like I was wrong. That capacitor I removed still offers up almost exactly the uf value on the tin. So that was another dead end. Hmm... One weird thing, all of the test points register 60Hz but not 110V. So thankfully the PSU isn't pushing wall socket voltage through. But that frequency is weird. My multimeter needs a charge though so I'll measure that again after it has.

The entire power area for the APU offers almost no resistance to the ground plane which is worrying. Again, need to charge that multimeter and re-check.


later again

Power on with no heatsink, the processor doesn't even warm to the touch. CPU, GPU, and other test points around the board pulse to 1-2V and then turn off fast.

Can't help but think it's related to the very low impedance between ground and positive on the V rails for the CPU/GPU. Is that normal?

USB port is charging the multimeter image

So that 5V rail from the southbridge is working.

Lots of 12V test points are consistently 12V (11.94V)


So...

Does any one have a diagram of the test points around the motherboard? What voltages / values should I be seeing? What are some likely culprits?

Thanks in advance! You're all wonderful!

 

This is the original XBOX One. Similar, but not exactly what I need. I can still maybe work from it.

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 8 years ago in reply to lilithelotor +5 suggested
    Sorry - I've been quite busy and am at work ... supposing you didn't lift any traces or warp the board significantly, you might well be fine. However, that's not to say that the VRM didn't fail for other…
  • lilithelotor
    lilithelotor over 8 years ago in reply to Gough Lui +4 suggested
    You are so wonderful and I can't thank you enough. I will work patiently from now on and I have learned a lot from this process. It is actually the first time I have ever used my hot air rework station…
  • Gough Lui
    Gough Lui over 8 years ago +3 suggested
    Most of the time, VRM issues are blown MOSFETs which have become shorted - your low resistance measurement is suggestive that the MOSFET on that phase may have gone shorted. Short burst of voltage and…
Parents
  • Gough Lui
    0 Gough Lui over 8 years ago

    Most of the time, VRM issues are blown MOSFETs which have become shorted - your low resistance measurement is suggestive that the MOSFET on that phase may have gone shorted. Short burst of voltage and shut down may be the converter going into protection due to overcurrent detection or because the shorted MOSFET may have tripped an upstream over-current protection.

     

    There's no easy way to test the MOSFET in circuit (to my knowledge, at least), but I would suggest replacing it and seeing what happens. It seems unlikely that the CPU/GPU itself is shorted since the other phases seem to measure a more reasonable resistance.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • lilithelotor
    0 lilithelotor over 8 years ago in reply to Gough Lui

    Gough Lui I'm having the hardest time searching for replacement MOSFETs. It would be great to even find a data sheet on these things. Probably not likely to happen. I bet it's a random manufacturer. (Unbranded.) But I could be wrong.

     

    Anyway, do you have any tips on trying to figure this out?

    [edit] OH! The big one is a 4055N and not a 4C55N. That helps a bit...
    [edit again] Oh! https://media.digikey.com/pdf/Data%20Sheets/ON%20Semiconductor%20PDFs/NTMFS4C55N.PDF  Maybe it -is- a C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lilithelotor
    0 lilithelotor over 8 years ago in reply to lilithelotor

    I found them! I will order them in a week or two. Found both on Mouser and only one of them on Digikey. Digikey had both but one was only in whole reel form. I do not need $2k or $4k worth of MOSFETs.

     

    Gough Lui Can you take a look at what I did?  https://www.youtube.com/watch?v=4XZNdUTsuTc

     

    I made a real mess but I think this is recoverable. Maybe once I get a few known good MOSFETs it'll work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 8 years ago in reply to lilithelotor

    Sorry - I've been quite busy and am at work ... supposing you didn't lift any traces or warp the board significantly, you might well be fine. However, that's not to say that the VRM didn't fail for other reasons (e.g. overloading due to a faulty CPU or shorted semiconductor is also possible).

     

    That being said, I only had the time to jump around your video - for such boards it pays to:

    - Be Patient - the board is designed with many vias to take heat away from the MOSFETs and use the copper planes as heatsinks. Hence if using hot air from the top, it can take a while to get things melted.

    - Use Additional Heat - if you have access to a hotplate of sorts, it could pay to rest the board on top of it so that it gets heated from the other side as well. This reduces the possibility of warpage of the board (which can stress the traces and other BGA joints) as well as reduce the thermal energy required to melt the solder.

    - Use Flux - mainly to conduct the heat slightly better and keep oxidation at bay - just remember to clean it off properly.

    - Don't Scratch - scrubbing with the tweezers is asking for trouble - applying pressure before it's ready risks lifting pads, scratches components and potentially also scratches adjacent traces on a slip of the tip.

     

    Resoldering the new MOSFETs will take some very careful work - the problem is the amount of solder required. On manufacturing lines, solder paste is pushed through stencils to leave a very precise amount which allows for the rear heat-sinking contact and all electrical contacts to make good contact. When applying by hand, it's very hard to achieve consistency - and if just pre-tinning the pads and reflowing, you will need flux and hope that you didn't supply too much/too little solder or too little heat resulting in a solder void on the thermal conduction pad (as the MOSFET could then cook and overheat).

     

    - Gough

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 8 years ago in reply to lilithelotor

    Sorry - I've been quite busy and am at work ... supposing you didn't lift any traces or warp the board significantly, you might well be fine. However, that's not to say that the VRM didn't fail for other reasons (e.g. overloading due to a faulty CPU or shorted semiconductor is also possible).

     

    That being said, I only had the time to jump around your video - for such boards it pays to:

    - Be Patient - the board is designed with many vias to take heat away from the MOSFETs and use the copper planes as heatsinks. Hence if using hot air from the top, it can take a while to get things melted.

    - Use Additional Heat - if you have access to a hotplate of sorts, it could pay to rest the board on top of it so that it gets heated from the other side as well. This reduces the possibility of warpage of the board (which can stress the traces and other BGA joints) as well as reduce the thermal energy required to melt the solder.

    - Use Flux - mainly to conduct the heat slightly better and keep oxidation at bay - just remember to clean it off properly.

    - Don't Scratch - scrubbing with the tweezers is asking for trouble - applying pressure before it's ready risks lifting pads, scratches components and potentially also scratches adjacent traces on a slip of the tip.

     

    Resoldering the new MOSFETs will take some very careful work - the problem is the amount of solder required. On manufacturing lines, solder paste is pushed through stencils to leave a very precise amount which allows for the rear heat-sinking contact and all electrical contacts to make good contact. When applying by hand, it's very hard to achieve consistency - and if just pre-tinning the pads and reflowing, you will need flux and hope that you didn't supply too much/too little solder or too little heat resulting in a solder void on the thermal conduction pad (as the MOSFET could then cook and overheat).

     

    - Gough

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • lilithelotor
    0 lilithelotor over 8 years ago in reply to Gough Lui

    You are so wonderful and I can't thank you enough.

     

    I will work patiently from now on and I have learned a lot from this process. It is actually the first time I have ever used my hot air rework station for its intended purpose. Before this I only used it to "reball" a MacBook Pro my friend owned. I got it working, amazingly!

     

    My plan is to buy about 5 of each of the 2 kinds of MOSFET and try replacing those, as well as maybe 10 of those capacitors. That way I have plenty of parts.

     

    My strategy will be to replace one MOSFET, test continuity to ground. If still low, replace another. Keep going until the issue goes away.

     

    I will probably not post again until the end of the month as I promised my partner I would not buy more parts from eBay for the rest of the month. (I think buying parts at all counts so I will be on hiatus.) image

    Thanks again! I appreciate your guidance SO MUCH!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 8 years ago in reply to lilithelotor

    Another thing I forgot to mention - MOSFETs are very sensitive to over-voltage stress, and an extension of this is that they are very susceptible to ESD damage. Do avoid handling the chips with bare hands too much and work in an ESD protected environment as much as possible.

     

    If you want to do things in parts, that's okay - but given the relatively low cost of the MOSFET and the potential that a shorted MOSFET could cause out-of-spec output every time you try to boot the unit, my philosophy is to "rework on a roll". Once you establish a pattern, it's much quicker to just do the whole lot (good or bad) in one sitting with the board still heated etc. This avoids thermal cycling which stresses the board, wasted time from downing tools and starting up again, and potentially more oxidation of solder from sitting at high temperatures after the initial good solder joint has been formed.

     

    Also remember to clear the pads well - you may well be working with leaded solder whereas the board would have been manufactured lead-free. Mixing the two often results in matte-looking, sometimes brittle joints.

     

    Good luck!

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer