Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum where to source silicon steel transformer winding kit.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 310 subscribers
  • Views 1127 views
  • Users 0 members are here
  • transformer design
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

where to source silicon steel transformer winding kit.

pdobson
pdobson over 7 years ago

I am trying to design a small transformer 3VA approx 12v input that will work at 400Hz. Is there anywhere I can buy a core kit including laminates and winding bobins??

BR Pete D.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago +2 suggested
    Farnell used to sell kits but don't seem to now. These people quote smallish quantities. https://www.edcorusa.com/ The two UK sources below may not sell in small quantities - they don't have very inspiring…
  • pdobson
    pdobson over 7 years ago in reply to michaelkellett +2
    Hi Mike, Thank you very much for you valued information. I have been trying to source these types of components on and off for several months. I do remember when Farnell used to sell them. The transformers…
  • pdobson
    pdobson over 7 years ago in reply to dougw +1 suggested
    Well, they are still very much used in the aviation industry today . My project is actually in building flight simulator instrument panels using as realistic instrumentation as is possible. This is a mix…
Parents
  • michaelkellett
    0 michaelkellett over 7 years ago

    Farnell used to sell kits but don't seem to now.

     

    These people quote smallish quantities.

    https://www.edcorusa.com/

     

     

    The two UK sources below may not sell in small quantities - they don't have very inspiring web sites.

     

     

    ASCO Components - Transformer Laminations, Bobbins, Angles, Frames, Terminals and Enclosures.

     

    L&H components ltd

     

     

    There are audio transformer kits on ebay that might do.

     

    https://www.ebay.co.uk/itm/Ni80-ee24-25-laminations-bobbin-DIY-premium-audio-transformer-x2/123006494304?_trkparms=aid%3…

     

    or you could buy a small transformer and re-wind it - use a toroid or dual bobbin type. If you start with a 12V 50Hz transformer you can cut down the number of turns by about 2.8 times for 400Hz working. Try to find one that is not varnish or plastic potted.

     

    What do you need it for ?

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 7 years ago

    Farnell used to sell kits but don't seem to now.

     

    These people quote smallish quantities.

    https://www.edcorusa.com/

     

     

    The two UK sources below may not sell in small quantities - they don't have very inspiring web sites.

     

     

    ASCO Components - Transformer Laminations, Bobbins, Angles, Frames, Terminals and Enclosures.

     

    L&H components ltd

     

     

    There are audio transformer kits on ebay that might do.

     

    https://www.ebay.co.uk/itm/Ni80-ee24-25-laminations-bobbin-DIY-premium-audio-transformer-x2/123006494304?_trkparms=aid%3…

     

    or you could buy a small transformer and re-wind it - use a toroid or dual bobbin type. If you start with a 12V 50Hz transformer you can cut down the number of turns by about 2.8 times for 400Hz working. Try to find one that is not varnish or plastic potted.

     

    What do you need it for ?

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • pdobson
    0 pdobson over 7 years ago in reply to michaelkellett

    Hi Mike,

     

    Thank you very much for you valued information. I have been trying to source these types of components on and off for several months. I do remember when Farnell used to sell them.

    The transformers I want to build are for use with Synchros and Resolvers as a hobby project. I have built a resolver reader interface card which generate sin/cos at 400Hz. works very well on 2 phase synchros, but I also use 3 phase resolver too and wanted to drive them from the same interface card. I can achieve this if I can translate the sin/cos drive to be 60 degrees apart instead of 90 and then ground the third pin of the 3 phase resolver. This produces three rotating vectors all 120 degrees apart. So the transformer is a sort of Scott connection (Modified) that feed a bit of the Sin channel into the Cos channel thus changing the 90 degree phase angle to 60 degrees. The winding ratios need to be accurate and I have not found anything off the shelf that can do the job so decided to wind my own.

    But first I need to acquire some core kits, I'll be on it first thing Monday morning.

     

    Thank you again for your help.

     

    BR Pete D.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to pdobson

    Wow, it has been a long time since I even heard anyone talking about synchros and resolvers. I hope you blog about your project here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pdobson
    0 pdobson over 7 years ago in reply to dougw

    Well, they are still very much used in the aviation industry today image .

     

    My project is actually in building flight simulator instrument panels using as realistic instrumentation as is possible. This is a mix of conventional clockwork instruments and modern EFIS displays. Last year I got my hands on three sets of professional Frasca instruments and the interface for these instruments covers a very broad range of technologies. Air Core motors, Standard DC brushed motors, stepper motors, you name it they are there somewhere. On the sensor side either Sychros are used or multi turn Linear resistance Potentiometers. I threw away the 1970s electronics and designed my own from scratch using Arduinos.

    I have an aviation background but have really enjoyed getting these all to work properly. Great fun when they do..............

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to pdobson

    Sounds like an awesome project. It would definitely be interesting to see some pictures as you progress.