Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum BASIC translation to Python
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 48 replies
  • Answers 24 answers
  • Subscribers 337 subscribers
  • Views 12515 views
  • Users 0 members are here
  • translation
  • python
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

BASIC translation to Python

tommy2k19
tommy2k19 over 7 years ago

I have written a few very basic programs in Python but have not done much program translation.

My friend asked me to translate his heating program from Basic to Python.

Is there an easy way to do this? I haven't tried anything yet?

 

Tha Basic code is below:

 

1:PRINT"HLOSS85.1":PRINT"":GOTO 3

 

3:"N"INPUT"INPUT NOTES> ";B$(0):PRINT B$(0):GOTO 3

 

4:PRINT "":IF L>0 END

 

5:GOSUB 9:GOTO 104

 

9:PRINT"------------------------":RETURN

 

10:"=" PRINT=LPRINT:PRINT"":END

 

20"L"PRINT=PRINT:PAUSE "PO":END

 

50:"S" CLEAR:USING

 

60:DIM B$(0)*24

 

70:DIM S(6),W(6),G(6),V(0),Z(0),P(0),Q(0),O(0),K(0),N(0):N=1:A(27)=25:R=25:T=600

 

80:M=21:J=-4:U=5.6:A(30)=55:A(32)=3:GOSUB 9:GOTO 1

 

104:INPUT"INPUT OUTSIDE TEMP C ";J

 

105:PRINT"OUTSIDE TEMP ";J;" C

 

106:INPUT"INPUT ROOM TEMP C ";M

 

107:C=M-J

 

108:PRINT"PRINT TEMP ";M;" C":PRINT"TD = ";C;" C

 

114: GOSUB 9

 

115:"C"B$(0)="":INPUT"INPUT ROOM NAME ";B$(0)

 

116:IF B$(0)="" GOTO 115

 

117:IF B$(0)="*" GOTO 320

 

120:PRINT B$(0)

 

125:Y$="N":INPUT"SAME AS LAST ROOM? ";Y$;:IF Y$="Y" GOTO 252

 

130:S(5)=0:P=0:Q=0:B=0:O=0:K=0k:V=0:O(0)=0:K(0)=0:A=0:G(5)=0:W=0

 

140:USING:L=0:W=0:H=0:INPUT"INPUT ROOM LENGTH M ";L,"INPUT WIDTH M ";W,"INPUT HEIGHT M ";H

 

165:Z=LW:V=ZH:IF V=0 GOTO 140

 

175:PRINT"L=";L;"M W=";W;"M H=";H;"M

 

176:PRINT"AREA ";Z;" M2

 

177:PRINT"VOLUME ";V; M3

 

180:S=1

 

190:S(S)=LH:GOSUB 500

 

200:S(S)=WH:GOSUB 500

 

210:S(S)=S(1):GOSUB 500

 

220:S(S)=S(2):GOSUB 500

 

230:S(S)=LW:GOSUB 500

 

240:S(S)=S(5):GOSUB 500

 

245:USING:D=M-J:INPUT"INPUT AC/HR ";N;"INPUT TD C ";D

 

246:PRINT N;" A/C @ ";D;" C TD":B=.33VND

 

247:INPUT"INPUT SAFETY % ";A(33)

 

248:IF A(33)>100 GOTO 247

 

249:A(36)=INT B+INT P+INT Q

 

250:A(34)=INT((A(33)/100)*A(36))

 

251:PRINT"SAFETY ";A(33);"% ";INT A(34);"W

 

252:K=INT A(34)+INT A(36)

 

253:Y$="":INPUT"IS INFO CORRECT ? ";Y$

 

254:IF Y$="N" GOTO 115

 

255:IF Y$<>"Y" GOTO 253

 

256:Z(0)=S(5)+Z(0):P(0)=INT P+P(0):Q(0)=INT Q+Q(0):V(0)=INT B+V(0);O(0)=O+O(0)

 

257:N(0)=V+N(0):K(0)+K+K(0):A(35)=A(34)+A(35)

 

258:PRINT"- ROOM HEAT LOSS -

 

260:PRINT"FABRIC ";INT Q;"W":PRINT"WINDOW ";INT P;"W":PRINT" VENT ";INT B;"W

 

261:PRINT"SAFETY ";INT A(34);"W

 

262:PRINT"TOTAL ROOM LOSS ";K;"W

 

263:IF V=0 GOTO 265

 

264:PRINT INT ((K/V)+.5);" W/M3

 

265:GOSUB 9

 

266:"H"USING:INPUT"INPUT RADIATOR HT MM ";T

 

267:PRINT"RAD HEIGHT ";T;"MM

 

268:PRINT"SINGLE ";INT(544K/T);"MM LENGTH

 

269:PRINT"DOUBLE ";INT(362/T);"MM

 

270:GOSUB 9

 

310:GOTO 115

 

320:PRINT"

 

330:"G"USING:PRINT:PRINT"-------- TOTALS --------

 

350:PRINT"FLOOR AREA ";Z(0);" M2

 

355:PRINT"VOLUME ";N(0);" M3

 

410:PRINT"FABRIC LOSS ";INT Q(0);"W

 

420:PRINT"WINDOW LOSS ";INT P(0);"W

 

430:PRINT"VENT LOSS ";INT V(0);"W

 

440:PRINT"SAFETY LOSS ";INT A(35);"W

 

457:GOSUB 9

 

460;K=INT Q(0)+INT P(0)+INT V(0)+ INT A(35):PRINT "TOTAL LOSS ";INT K;"W

 

465:PRINT"AV.HEAT LOSS ";INT((K/M-J))+.5);"W/C

 

467:IF N(0)=0 GOTO 480

 

468:PRINT" ";INT((K/N(0)))+.5);"W/M3

 

470:PRINT USING"###.##";"G VALUE ";(K/(M-J))/N(0);" W/M3/C

 

480:USING:GOSUB 9

 

484:GOTO 900

 

489:A(31)=K+A(29)*1E3

 

490:INPUT"INPUT BOILER MARGIN % ";A(27)

 

491:A(28)=A(31)*A(27)/1E2

 

492:PRINT"BOILER MARGIN":PRINT A(27);"% = ";INT A(28);"W

 

493:GOSUB 9

 

494:PRINT" BOILER SIZE

 

495:PRINT USING"#######.#";" ";(A(31)+A(28))/1E3;"KW

 

496:USING:GOSUB 9

 

497:PRINT "":PRINT"

 

498:END

 

500:IF S<5 PRINT"WALL ";S

 

502:IF S=5 PRINT"CEILING/ROOF

 

504:IF S=6 PRINT"FLOOR

 

505:X=0:G(S)=0:C=M-J

 

507:INPUT"INPUT FABRIC U VALUE ";X:GOTO 509

 

508:GOTO 515

 

509:INPUT"INPUT TD C";C

 

510:GOSUB 700

 

512:IF X>0 GOTO 530

 

515:PRINT"NO LOSS

 

530:S=S+1:RETURN

 

700:IF S<6 INPUT"INPUT GLASS AREA M2 ";G(S)

 

702:IF G(S)>S(S) GOTO 700

 

705:W(S)=S(S)-G(S):IF W(S)=S(S) GOTO 710

 

707:IF S<5 LET A=A+S(S)

 

710:F=W(S)CX:PRINT W(S);"X";X;"X";C;"=";F;"W

 

712:Q=Q+F

 

715:IF S(S)=W(S) RETURN

 

717:INPUT"INPUT GLASS U VALUE ";U

 

800:IF S=5 PRINT"ROOFLIGHT":GOTO 805

 

802:PRINT"WINDOW ";S

 

805:G=G(S)UC

 

810:PRINT G(S);"X";U;"X";C;"=";G;"W

 

815:P=P+G:O=O+G(S)

 

820:K(0)=G(5)

 

830:RETURN

 

900:"D"USING:PRINT"D.H.WATER":INPUT"INPUT NO.OF PEOPLE ";I

 

905:IF I>0 PRINT 920

 

910:A(29)=0:PRINT"NONE":GOTO 489

 

920:INPUT"INPUT LITRE/PERSON ";R

 

930:PRINT I;"PEOPLE X ";R;"LITRE

 

940:INPUT"INPUT WARMUP - HRS ";A(32)

 

942:INPUT"INPUT WATER TD C ";A(30)

 

945:A(29)=4.2A(A30)IR/3600A(32)

 

950:PRINT A(32);"HR WARMUP @ ";A(30);"C TD

 

955:PRINT USING"#####.#";HOT WATER CYL";A(29);"KW

 

970:USING:GOTO 489

 

975:"X"USING:INPUT"INPUT FLOOR AREA M2";Z(0):PRINT Z(0)

 

976:INPUT"INPUT VOLUME M3 ";N(0):PRINT N(0)

 

977:INPUT"INPUT FABRIC W ";Q(0):PRINT Q(0)

 

978:INPUT"INPUT WINDOW W ";P(0):PRINT P(0)

 

979:INPUT"INPUT VENT W "V(0):PRINT V(0)

 

980:INPUT"INPUT SAFETY W ";A(35):PRINT A(35)

 

995:GOTO "G"

 

997:"Z"INPUT"INPUT W";K:PRINT K;"W

 

998:GOTO "H"

  • Cancel

Top Replies

  • jomoenginer
    jomoenginer over 7 years ago in reply to tommy2k19 +4 suggested
    There is no GOTO or GOSUB in Python. It is used in C but discouraged in most cases; it is quite common in BASIC. You can think of a GOTO as in an if-elif-else case or just replace the GOTO from BASIC with…
  • jomoenginer
    jomoenginer over 7 years ago in reply to Jan Cumps +4
    Jan Cumps wrote: If it’s a good friend, show this thread. If it is not a very good friend, show the thread then run away . Or it would completely offend the friend and create a negative view of the folks…
  • jc2048
    jc2048 over 7 years ago in reply to Jan Cumps +4 suggested
    The Sharp 1251 seems to have been sold by Tandy rebadged as the PC-3. There's a user manual here that includes a reference for their version of BASIC. https://ia601707.us.archive.org/13/items/PC-3_Owners_Manual_19xx_Tandy…
Parents
  • Jan Cumps
    0 Jan Cumps over 7 years ago

    I'd first try to find out if there's logic in the basis code, and try to understand what it's doing.

    You could:

    - draw the program logic, based on the basis program

    - GOSUBs become functions

    - fiddle out what the flow of the GOTOs does.

     

    Then do the translation, function per function.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 7 years ago

    I'd first try to find out if there's logic in the basis code, and try to understand what it's doing.

    You could:

    - draw the program logic, based on the basis program

    - GOSUBs become functions

    - fiddle out what the flow of the GOTOs does.

     

    Then do the translation, function per function.