Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum BASIC translation to Python
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Locked Locked
  • Replies 48 replies
  • Answers 24 answers
  • Subscribers 337 subscribers
  • Views 12456 views
  • Users 0 members are here
  • translation
  • python
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

BASIC translation to Python

tommy2k19
tommy2k19 over 7 years ago

I have written a few very basic programs in Python but have not done much program translation.

My friend asked me to translate his heating program from Basic to Python.

Is there an easy way to do this? I haven't tried anything yet?

 

Tha Basic code is below:

 

1:PRINT"HLOSS85.1":PRINT"":GOTO 3

 

3:"N"INPUT"INPUT NOTES> ";B$(0):PRINT B$(0):GOTO 3

 

4:PRINT "":IF L>0 END

 

5:GOSUB 9:GOTO 104

 

9:PRINT"------------------------":RETURN

 

10:"=" PRINT=LPRINT:PRINT"":END

 

20"L"PRINT=PRINT:PAUSE "PO":END

 

50:"S" CLEAR:USING

 

60:DIM B$(0)*24

 

70:DIM S(6),W(6),G(6),V(0),Z(0),P(0),Q(0),O(0),K(0),N(0):N=1:A(27)=25:R=25:T=600

 

80:M=21:J=-4:U=5.6:A(30)=55:A(32)=3:GOSUB 9:GOTO 1

 

104:INPUT"INPUT OUTSIDE TEMP C ";J

 

105:PRINT"OUTSIDE TEMP ";J;" C

 

106:INPUT"INPUT ROOM TEMP C ";M

 

107:C=M-J

 

108:PRINT"PRINT TEMP ";M;" C":PRINT"TD = ";C;" C

 

114: GOSUB 9

 

115:"C"B$(0)="":INPUT"INPUT ROOM NAME ";B$(0)

 

116:IF B$(0)="" GOTO 115

 

117:IF B$(0)="*" GOTO 320

 

120:PRINT B$(0)

 

125:Y$="N":INPUT"SAME AS LAST ROOM? ";Y$;:IF Y$="Y" GOTO 252

 

130:S(5)=0:P=0:Q=0:B=0:O=0:K=0k:V=0:O(0)=0:K(0)=0:A=0:G(5)=0:W=0

 

140:USING:L=0:W=0:H=0:INPUT"INPUT ROOM LENGTH M ";L,"INPUT WIDTH M ";W,"INPUT HEIGHT M ";H

 

165:Z=LW:V=ZH:IF V=0 GOTO 140

 

175:PRINT"L=";L;"M W=";W;"M H=";H;"M

 

176:PRINT"AREA ";Z;" M2

 

177:PRINT"VOLUME ";V; M3

 

180:S=1

 

190:S(S)=LH:GOSUB 500

 

200:S(S)=WH:GOSUB 500

 

210:S(S)=S(1):GOSUB 500

 

220:S(S)=S(2):GOSUB 500

 

230:S(S)=LW:GOSUB 500

 

240:S(S)=S(5):GOSUB 500

 

245:USING:D=M-J:INPUT"INPUT AC/HR ";N;"INPUT TD C ";D

 

246:PRINT N;" A/C @ ";D;" C TD":B=.33VND

 

247:INPUT"INPUT SAFETY % ";A(33)

 

248:IF A(33)>100 GOTO 247

 

249:A(36)=INT B+INT P+INT Q

 

250:A(34)=INT((A(33)/100)*A(36))

 

251:PRINT"SAFETY ";A(33);"% ";INT A(34);"W

 

252:K=INT A(34)+INT A(36)

 

253:Y$="":INPUT"IS INFO CORRECT ? ";Y$

 

254:IF Y$="N" GOTO 115

 

255:IF Y$<>"Y" GOTO 253

 

256:Z(0)=S(5)+Z(0):P(0)=INT P+P(0):Q(0)=INT Q+Q(0):V(0)=INT B+V(0);O(0)=O+O(0)

 

257:N(0)=V+N(0):K(0)+K+K(0):A(35)=A(34)+A(35)

 

258:PRINT"- ROOM HEAT LOSS -

 

260:PRINT"FABRIC ";INT Q;"W":PRINT"WINDOW ";INT P;"W":PRINT" VENT ";INT B;"W

 

261:PRINT"SAFETY ";INT A(34);"W

 

262:PRINT"TOTAL ROOM LOSS ";K;"W

 

263:IF V=0 GOTO 265

 

264:PRINT INT ((K/V)+.5);" W/M3

 

265:GOSUB 9

 

266:"H"USING:INPUT"INPUT RADIATOR HT MM ";T

 

267:PRINT"RAD HEIGHT ";T;"MM

 

268:PRINT"SINGLE ";INT(544K/T);"MM LENGTH

 

269:PRINT"DOUBLE ";INT(362/T);"MM

 

270:GOSUB 9

 

310:GOTO 115

 

320:PRINT"

 

330:"G"USING:PRINT:PRINT"-------- TOTALS --------

 

350:PRINT"FLOOR AREA ";Z(0);" M2

 

355:PRINT"VOLUME ";N(0);" M3

 

410:PRINT"FABRIC LOSS ";INT Q(0);"W

 

420:PRINT"WINDOW LOSS ";INT P(0);"W

 

430:PRINT"VENT LOSS ";INT V(0);"W

 

440:PRINT"SAFETY LOSS ";INT A(35);"W

 

457:GOSUB 9

 

460;K=INT Q(0)+INT P(0)+INT V(0)+ INT A(35):PRINT "TOTAL LOSS ";INT K;"W

 

465:PRINT"AV.HEAT LOSS ";INT((K/M-J))+.5);"W/C

 

467:IF N(0)=0 GOTO 480

 

468:PRINT" ";INT((K/N(0)))+.5);"W/M3

 

470:PRINT USING"###.##";"G VALUE ";(K/(M-J))/N(0);" W/M3/C

 

480:USING:GOSUB 9

 

484:GOTO 900

 

489:A(31)=K+A(29)*1E3

 

490:INPUT"INPUT BOILER MARGIN % ";A(27)

 

491:A(28)=A(31)*A(27)/1E2

 

492:PRINT"BOILER MARGIN":PRINT A(27);"% = ";INT A(28);"W

 

493:GOSUB 9

 

494:PRINT" BOILER SIZE

 

495:PRINT USING"#######.#";" ";(A(31)+A(28))/1E3;"KW

 

496:USING:GOSUB 9

 

497:PRINT "":PRINT"

 

498:END

 

500:IF S<5 PRINT"WALL ";S

 

502:IF S=5 PRINT"CEILING/ROOF

 

504:IF S=6 PRINT"FLOOR

 

505:X=0:G(S)=0:C=M-J

 

507:INPUT"INPUT FABRIC U VALUE ";X:GOTO 509

 

508:GOTO 515

 

509:INPUT"INPUT TD C";C

 

510:GOSUB 700

 

512:IF X>0 GOTO 530

 

515:PRINT"NO LOSS

 

530:S=S+1:RETURN

 

700:IF S<6 INPUT"INPUT GLASS AREA M2 ";G(S)

 

702:IF G(S)>S(S) GOTO 700

 

705:W(S)=S(S)-G(S):IF W(S)=S(S) GOTO 710

 

707:IF S<5 LET A=A+S(S)

 

710:F=W(S)CX:PRINT W(S);"X";X;"X";C;"=";F;"W

 

712:Q=Q+F

 

715:IF S(S)=W(S) RETURN

 

717:INPUT"INPUT GLASS U VALUE ";U

 

800:IF S=5 PRINT"ROOFLIGHT":GOTO 805

 

802:PRINT"WINDOW ";S

 

805:G=G(S)UC

 

810:PRINT G(S);"X";U;"X";C;"=";G;"W

 

815:P=P+G:O=O+G(S)

 

820:K(0)=G(5)

 

830:RETURN

 

900:"D"USING:PRINT"D.H.WATER":INPUT"INPUT NO.OF PEOPLE ";I

 

905:IF I>0 PRINT 920

 

910:A(29)=0:PRINT"NONE":GOTO 489

 

920:INPUT"INPUT LITRE/PERSON ";R

 

930:PRINT I;"PEOPLE X ";R;"LITRE

 

940:INPUT"INPUT WARMUP - HRS ";A(32)

 

942:INPUT"INPUT WATER TD C ";A(30)

 

945:A(29)=4.2A(A30)IR/3600A(32)

 

950:PRINT A(32);"HR WARMUP @ ";A(30);"C TD

 

955:PRINT USING"#####.#";HOT WATER CYL";A(29);"KW

 

970:USING:GOTO 489

 

975:"X"USING:INPUT"INPUT FLOOR AREA M2";Z(0):PRINT Z(0)

 

976:INPUT"INPUT VOLUME M3 ";N(0):PRINT N(0)

 

977:INPUT"INPUT FABRIC W ";Q(0):PRINT Q(0)

 

978:INPUT"INPUT WINDOW W ";P(0):PRINT P(0)

 

979:INPUT"INPUT VENT W "V(0):PRINT V(0)

 

980:INPUT"INPUT SAFETY W ";A(35):PRINT A(35)

 

995:GOTO "G"

 

997:"Z"INPUT"INPUT W";K:PRINT K;"W

 

998:GOTO "H"

  • Cancel

Top Replies

  • jomoenginer
    jomoenginer over 7 years ago in reply to tommy2k19 +4 suggested
    There is no GOTO or GOSUB in Python. It is used in C but discouraged in most cases; it is quite common in BASIC. You can think of a GOTO as in an if-elif-else case or just replace the GOTO from BASIC with…
  • jomoenginer
    jomoenginer over 7 years ago in reply to Jan Cumps +4
    Jan Cumps wrote: If it’s a good friend, show this thread. If it is not a very good friend, show the thread then run away . Or it would completely offend the friend and create a negative view of the folks…
  • jc2048
    jc2048 over 7 years ago in reply to Jan Cumps +4 suggested
    The Sharp 1251 seems to have been sold by Tandy rebadged as the PC-3. There's a user manual here that includes a reference for their version of BASIC. https://ia601707.us.archive.org/13/items/PC-3_Owners_Manual_19xx_Tandy…
Parents
  • balearicdynamics
    0 balearicdynamics over 7 years ago

    Jan Cumps says:

     

    GOTOs are things from 1970 image - I don't know if Python supports it.

    This is the key... What you say translation is porting. The difference is important. You can translate a natural language to another when both refer to the same or similar cultural background, like English to French or German or Spanis. When the two languages refer to totally different cultures, you can't translate. Not literally. You should contextualize the meaning of one language and convert it to a different cultural reference that for the reader has the same or similar meaning., as well as with artificial languages.

     

    So, porting means that you should understand very well the logic and behavior of the basic program, then rewrite it using a language based on a totally different semantics.

     

    Just as an example, the basic GOTO in the source you showed (it is the case you paste the code and select the syntax highlight for better readability) send from a point to another, executes a series of instructions then GOTO back from the origin. This means that in Python you should create a function, that is called in correspondence of every GOTO ... GOTO (back). Then analyzing the source may be that all the functions with similar behavior are collected in classes to make easier the understanding of the new approach. And so on...

     

    Enrico

     

     

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago in reply to balearicdynamics

    I could not say it better, balearicdynamics. Or almost not better image

     

    GOSUBs are like jump then return

    GOTOs are jump without a return point. Just jump.

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 7 years ago in reply to Jan Cumps

    Thank you Jan, you are right, about GOTO and GOSUB but it is important to see the context of the program. Sometime in the '70s, we were obliged to do not so elegant things to make the language working due to the memory limitations, processor speed, and many other factors. Then just to complete the scenario, we can't exclude that we don't know the knowledge level of the BASIC programmer. Maybe that nowadays a lot of this source can be optimized...

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago in reply to balearicdynamics

    This is so true, Enrico.

     

    Programming languages have continuously been evolving (or - in the case of Python - devolving image ) .

    You can never critique a programming style when the development was done before we were able to learn from the limitations.

    There are good programs written in BASIC with GOTOs.

    Unfortunately for tommy2k19, the code he got from his friend is not one of those. It's not a thankful job to have to port this code.

    I think it's made ad-hoc, and it seems that it has been done by several people (I see 2 programming styles: the early GOTO style and the later GOSUB style).

     

    If I had to adapt this code as a consultant, I would do it, but I would charge a bigger fee as usual because I can't assess if the logic is sound from reading the code.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 7 years ago in reply to Jan Cumps

    As a matter of fact, I see the program is short, so the algorithm can't be extremely complex. Under this perspective, IMHO it is better a good description and – eventually – a flow to rewrite the things instead of a bare porting...

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 7 years ago in reply to Jan Cumps

    As a matter of fact, I see the program is short, so the algorithm can't be extremely complex. Under this perspective, IMHO it is better a good description and – eventually – a flow to rewrite the things instead of a bare porting...

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
Children
No Data