Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Desoldering Iron STand
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 5 answers
  • Subscribers 340 subscribers
  • Views 2563 views
  • Users 0 members are here
  • desoldering
  • stand
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Desoldering Iron STand

rickseiden
rickseiden over 6 years ago

Hello,

 

I have one of those desoldering irons with a vacumm bulb on it.  Like this one from Newark.

 

desoldering iron

 

I can't find a way to store it when it's hot.  There are a ton of soldering iron stands, but they are all too skinny to fit this thing into them.

 

Does anyone have one or know of one that I can pick up?

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago in reply to rickseiden +5 suggested
    I guess it needs to be anchored into a solid base. Maybe a ceramic gravy boat would work without any need for fabrication … or a coat hanger inside a gravy boat wouldn't tip.
  • jw0752
    jw0752 over 6 years ago in reply to colporteur +3 suggested
    Hi Sean, I can't speak for Douglas but it seems to tick off most off the practical conditions. It would provide a place to set the iron where the hot tip would not cause any damage. It looks stable so…
  • msebok
    msebok over 6 years ago +3 suggested
    What about something like this? https://media-weller.de/weller/data/Weller%20FT/images/T0051508099.jpg
Parents
  • clem57
    0 clem57 over 6 years ago

    My choice:

    Desoldering braid, also known as desoldering wick or solder wick, is finely braided 18 to 42 AWG copper wire coated with rosin flux, usually supplied on a roll. ... The connections are heated with a soldering iron until the solder melts and is wicked into the braid by capillary action.

    But to each is own...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 6 years ago

    My choice:

    Desoldering braid, also known as desoldering wick or solder wick, is finely braided 18 to 42 AWG copper wire coated with rosin flux, usually supplied on a roll. ... The connections are heated with a soldering iron until the solder melts and is wicked into the braid by capillary action.

    But to each is own...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer