Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Differences between active and passive components
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 322 subscribers
  • Views 449 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Differences between active and passive components

s.a.ayoola
s.a.ayoola over 6 years ago

How do active components produce power in terms of current or voltage

  • Sign in to reply
  • Cancel
Parents
  • colporteur
    0 colporteur over 6 years ago

    Using a transistor, as an example of an active component, has the potential to modify the current or voltage on its outputs compared to its input. A passive component like a resistor does not.

     

    A transistor used as a amplifier modifies the lower signal input to a higher signal output.

    image

    Without getting into a deep dive on active component technologies and how they are built to accomplish the task. Let's use the block diagram and think of the box as an active component. Any signal entering on the left side is modified by a factor of 5. 1V in become 1V out. The active components has amplified the signal.

     

    You could reverse the box and the active components is designed to reduce the signal.

     

    If the input signal was a varying sine wave the output would be a the sine was at a higher amplitude.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 6 years ago

    Using a transistor, as an example of an active component, has the potential to modify the current or voltage on its outputs compared to its input. A passive component like a resistor does not.

     

    A transistor used as a amplifier modifies the lower signal input to a higher signal output.

    image

    Without getting into a deep dive on active component technologies and how they are built to accomplish the task. Let's use the block diagram and think of the box as an active component. Any signal entering on the left side is modified by a factor of 5. 1V in become 1V out. The active components has amplified the signal.

     

    You could reverse the box and the active components is designed to reduce the signal.

     

    If the input signal was a varying sine wave the output would be a the sine was at a higher amplitude.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data