Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Differential amplifier problem
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Answers 15 answers
  • Subscribers 326 subscribers
  • Views 11099 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Differential amplifier problem

Andrew J
Andrew J over 6 years ago

I'm working with a DAC and experimenting with removing the zero scale error - the actual output at a zero input code.  I'm on a breadboard so it isn't particularly accurate but the ZSE is 5mV to 11mV.

 

I set up a differential amplifier as follows - image is copied from a website, but I've confirmed and re-confirmed that my setup matches:

image

So, I have the following inputs:

V1 = 0.005mV

V2 = DACoutput

R = 100K.  All of them.

Opamp is an LM741 which is all I have on-hand, V+ = 5V, V- = ground .  It has a max offset voltage of 6mV.

 

Given that, I would expect Vout = V2 - V1.  Vout is connected to a 1K resistor to ground.

 

So the reality is that the R values are not perfectly 100K but are within the 10% spec.  Thus I wouldn't expect Vout to be an exact difference, but 'more-or-less'.

 

This is what I'm measuring:

DACout (V2) = 4.06V, Vout = 4.04V

DACout (V2) = 0.011V, Vout = 3.6V

 

I've tried working out why with a low DACout I'm still getting a large Vout.  Measuring the resistors and plugging them into the gain formula:

 

Vout = -0.005 * (99.03/99.5) + 0.011 * (99.21/(99.05+99.21)) * ((99.5+99.03)/99.5)

Vout = (-0.005 * 0.995) + (0.011 * 0.500 * 1.995)

Vout = -0.005 + 0.011 = 0.006

 

So, essentially, my calculation confirms what I would expect the amplifier to do with a -0.005mV and 0.011mV input.

 

I can't figure out where I've gone wrong, can anyone give me some pointers?

Attachments:
2477.LM741.asc.zip
  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +5 verified
    What power do you have connected to the 741 - it's not rail to rail capable it needs positive and negative supplies, +/- 10V is the minimum recommended. The input common mode range is +/- 12V when running…
  • michaelkellett
    michaelkellett over 6 years ago in reply to Andrew J +5 suggested
    If you want to sink any current at 0V you need a negative supply. You could consider using +/- 5V supplies (+/- 10 if you stick with the 741 ) You can do a lot of this without spending money by using a…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Andrew J +4 suggested
    Yes, we're doing it the naive way. That's why I hope that analog / DAC experts chime in and show the shining path to real world solutions. In the eLoad we made, things like OpAmp offset, quiescent current…
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    What power do you have connected to the 741 - it's not rail to rail capable it needs positive and negative supplies, +/- 10V is the minimum recommended.

    The input common mode range is +/- 12V when running with +/- 15V supplies - that means that the amp won't work properly if either input is closer to a supply rail than 3V.

     

    The LM741 was designed (by David Fullagar at  Fairchild) in 1968 - 52 years ago - we have better parts now image

     

    Just seen your photo - single rail supply ?

     

    The poor old 741 can't work like that, but you won't get any (even rail to rail IO types) op amp to do get the output right down to zero.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to michaelkellett

    Michael, if I understand what you are saying, trying to use an OpAmp of any sort to get rid of a, say, 5mV ZSE is not going to be possible?  My thought was a theoretical 0mV should be <1mV (uV in other words) rather than an actual 0V.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 6 years ago in reply to michaelkellett

    Michael, if I understand what you are saying, trying to use an OpAmp of any sort to get rid of a, say, 5mV ZSE is not going to be possible?  My thought was a theoretical 0mV should be <1mV (uV in other words) rather than an actual 0V.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to Andrew J

    The problem is this:

     

    Suppose you use an MCP4822 dual 12 bit DAC, the output offset max at zero code is +/- 1% of full scale = 20.48mV or 41 bits.

     

    A typical rail to rail input amplifier will have a common mode range that goes down to maybe 0.3V below ground (although performance may not be well specified there.)

     

    Your diff amp will be OK - the voltage on the positive input will be max 10mV to -10mV. To null that you'll need + or - 10mV on the other pin but there is a flaw in this reasoning !

     

    It won't work - think about that weasel spec, the code is zero and the offset is -20mV or -41 bits . But the DAC only has 0 - 5V supply rails - its output can't go negative !!

     

    So if you set any code in between 0 and 41 the DAC output just sits at 0V - so you can't null the zero offset of a single rail DAC.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to michaelkellett

    I had realised that I couldn't get rid of that 0 to 41 code range by software compensation; the output is never 0mV (or -ve) with this type of delta-sigma DAC, it's always positive in some form (as I understand from how these types of DACs work.)  The MCP4728 I use doesn't state a ZSE in the datasheet but the Offset error is 5mV (typical) to 20mV (max.)  At this point, I was looking at reducing it through the diff. amp such that, to take your example, 0 to 41 is 0mV, 42 becomes 1mV, 43 becomes 2 and so on.  I realise this is taken the full scale range further below where it currently sits because it will subtract 5mV from all output values.  In my actual case, that zero scale error was 5mV (or 11mV it's not always so stable on the breadboard) so I was trying to 'subtract' 5mV thus a code of 0 to 5 become 0V, 6 becomes 1mV and so on. 

     

    I'm not sure yet whether this is possible or not given what you've said, perhaps I'm still misunderstanding something?  Clearly I need something better than the op amp I have so thanks for clearing that up, that's been really useful.  I'll have a play around in LTSpice and see what I come up with.

     

    Thanks for the input.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to Andrew J

    What DAC are you using (and planning to use) - precision non audio DACs are almost never delta sigma types.

     

    (I'm going home now so won't see any more till tomorrow.)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to michaelkellett

    Yes, sorry, it's a resistor string architecture - I've been reading too much recently.  The DAC is an MCP4728 and I'm thinking of a ADS5694R-B or AD5696R-B (same datasheet as the ..4R-B)  These latter ones have a +Ve ZSE and a max +-1.5 offset error.

     

    It's the ADC I've been using, MCP3428, which is Sigma-Delta.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer