Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Differential amplifier problem
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Answers 15 answers
  • Subscribers 326 subscribers
  • Views 11110 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Differential amplifier problem

Andrew J
Andrew J over 6 years ago

I'm working with a DAC and experimenting with removing the zero scale error - the actual output at a zero input code.  I'm on a breadboard so it isn't particularly accurate but the ZSE is 5mV to 11mV.

 

I set up a differential amplifier as follows - image is copied from a website, but I've confirmed and re-confirmed that my setup matches:

image

So, I have the following inputs:

V1 = 0.005mV

V2 = DACoutput

R = 100K.  All of them.

Opamp is an LM741 which is all I have on-hand, V+ = 5V, V- = ground .  It has a max offset voltage of 6mV.

 

Given that, I would expect Vout = V2 - V1.  Vout is connected to a 1K resistor to ground.

 

So the reality is that the R values are not perfectly 100K but are within the 10% spec.  Thus I wouldn't expect Vout to be an exact difference, but 'more-or-less'.

 

This is what I'm measuring:

DACout (V2) = 4.06V, Vout = 4.04V

DACout (V2) = 0.011V, Vout = 3.6V

 

I've tried working out why with a low DACout I'm still getting a large Vout.  Measuring the resistors and plugging them into the gain formula:

 

Vout = -0.005 * (99.03/99.5) + 0.011 * (99.21/(99.05+99.21)) * ((99.5+99.03)/99.5)

Vout = (-0.005 * 0.995) + (0.011 * 0.500 * 1.995)

Vout = -0.005 + 0.011 = 0.006

 

So, essentially, my calculation confirms what I would expect the amplifier to do with a -0.005mV and 0.011mV input.

 

I can't figure out where I've gone wrong, can anyone give me some pointers?

Attachments:
2477.LM741.asc.zip
  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +5 verified
    What power do you have connected to the 741 - it's not rail to rail capable it needs positive and negative supplies, +/- 10V is the minimum recommended. The input common mode range is +/- 12V when running…
  • michaelkellett
    michaelkellett over 6 years ago in reply to Andrew J +5 suggested
    If you want to sink any current at 0V you need a negative supply. You could consider using +/- 5V supplies (+/- 10 if you stick with the 741 ) You can do a lot of this without spending money by using a…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Andrew J +4 suggested
    Yes, we're doing it the naive way. That's why I hope that analog / DAC experts chime in and show the shining path to real world solutions. In the eLoad we made, things like OpAmp offset, quiescent current…
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    What power do you have connected to the 741 - it's not rail to rail capable it needs positive and negative supplies, +/- 10V is the minimum recommended.

    The input common mode range is +/- 12V when running with +/- 15V supplies - that means that the amp won't work properly if either input is closer to a supply rail than 3V.

     

    The LM741 was designed (by David Fullagar at  Fairchild) in 1968 - 52 years ago - we have better parts now image

     

    Just seen your photo - single rail supply ?

     

    The poor old 741 can't work like that, but you won't get any (even rail to rail IO types) op amp to do get the output right down to zero.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to michaelkellett

    Wolfgang/Michael,

     

    it's using 5V+, 0V- so no -ve supply rail; I could run it from a 12V+ which would keep DACout max well below that limit.  I did wonder about a -Ve supply rail originally, but as I wasn't asking it to output a -ve voltage I didn't think it would matter.

     

    The LM741 is all I have to hand and was something I got hold of when I first started out learning this stuff.  I'm prototyping ideas at the moment before getting a prototype PCB made up.  One of my ideas involves buffering an ADC input so I had sort of settled on getting a OP388 for that and I'd thought if this zero code error compensation worked I would get another (OP4388) for that purpose.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to Andrew J

    If you want to sink any current at 0V you need a negative supply. You could consider using +/- 5V supplies (+/- 10 if you stick with the 741 image)

     

    You can do a lot of this without spending money by using a simulator - LTSpice is free and good - (from www.analog.com)

     

    The OP388 parts are interesting but they are chopper amps which means that they bring their own special problems and they are not that cheap.

     

    One (of many) things to be concerned about is that the DAC will be non linear at low outputs if its a single rail part !

     

    If you really want to play with actual parts rather than simulate then get some Microchip op amps (because some come in DIL packages).

     

    MCP6002 are dirt cheap, rail to rail IO, not too fast so won't be too hard to handle on bread board. Single rail max supply 6V.

    Offsets not that good but bias current is tiny.

    1292245 from Farnell at £0.26 for a dual op amp means you won't be too sad when you blow one.

     

    I'm not sure what your goal with this work is - if you can explain a bit more I might be able to offer more useful suggestions.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • wolfgangfriedrich
    0 wolfgangfriedrich over 6 years ago in reply to Andrew J

    I was going the same route as Michael, he already gave the correct hint in his question. image

     

    This is the relevant datasheet section for a +-15V supply:

    image

    And the 741 could not be run with +5V/0V at all:

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to michaelkellett

    Basically, I'm having a play around with DACs and ADCs creating my own version of Jan' and Peter's Boost board for their eload.  Ultimately, I'll probably add a DC load onto this as well but right now, I'm just trying to get a better understanding of these devices and how I might improve the output.  That's fairly simplistic because I am trying to make a control board with other things as well, but here is what I'm trying to do specifically with the DAC / ADC side of things.

     

    The 12-bit DAC, with a 4.096 external reference, I have is 'ok' - pretty cheap, not highly accurate and I will change it for another shortly - and I can measure it's output as 5mV to around 4.080V.  So there is a Zero Scale Error of around 5mV and a Full Scale Error of 26mV.  Sticking with the ZCE: what this means is that if I try and output codes 0 to 5 I get 5mV, 6 I get 6mV etc.  My idea was to use a differential amplifier with a 0.005mV input on the inverting side to 'subtract' this from the output of the DAC on the non-inverting side.

     

    The 16-bit ADC isn't too bad and I know that will come with its own errors.  I had thought I would buffer the ADC inputs with a simple RC filter on the buffer output to filter any noise.  For this, I had thought to use an OP388 as TI promote it for such a purpose:

    "The OPAx388 (OPA388, OPA2388, and OPA4388) series of precision operational amplifiers are ultra-low noise, fast-settling, zero-drift, zero-crossover devices that provide rail-to-rail input and output operation. These features and excellent ac performance, combined with only 0.25 μV of offset and 0.005 μV/°C of drift over temperature, makes the OPAx388 a great choice for driving high-precision, analog-to-digital converters (ADCs) or buffering the output of high- resolution, digital-to-analog converters (DACs). This design results in excellent performance when driving analog-to-digital converters (ADCs) without degradation of linearity."

     

    There are things that I don't yet understand but that's why I'm doing it - for fun and learning, so I don't mind spending a bit of money to work things out.  I'm trying some things I can do on a breadboard first and then reading around potential solutions for what I'm seeing.  At some point I want to actually produce a PCB because it's as cheap to do that as to get DIL adapters for the ICs!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 6 years ago in reply to michaelkellett

    Basically, I'm having a play around with DACs and ADCs creating my own version of Jan' and Peter's Boost board for their eload.  Ultimately, I'll probably add a DC load onto this as well but right now, I'm just trying to get a better understanding of these devices and how I might improve the output.  That's fairly simplistic because I am trying to make a control board with other things as well, but here is what I'm trying to do specifically with the DAC / ADC side of things.

     

    The 12-bit DAC, with a 4.096 external reference, I have is 'ok' - pretty cheap, not highly accurate and I will change it for another shortly - and I can measure it's output as 5mV to around 4.080V.  So there is a Zero Scale Error of around 5mV and a Full Scale Error of 26mV.  Sticking with the ZCE: what this means is that if I try and output codes 0 to 5 I get 5mV, 6 I get 6mV etc.  My idea was to use a differential amplifier with a 0.005mV input on the inverting side to 'subtract' this from the output of the DAC on the non-inverting side.

     

    The 16-bit ADC isn't too bad and I know that will come with its own errors.  I had thought I would buffer the ADC inputs with a simple RC filter on the buffer output to filter any noise.  For this, I had thought to use an OP388 as TI promote it for such a purpose:

    "The OPAx388 (OPA388, OPA2388, and OPA4388) series of precision operational amplifiers are ultra-low noise, fast-settling, zero-drift, zero-crossover devices that provide rail-to-rail input and output operation. These features and excellent ac performance, combined with only 0.25 μV of offset and 0.005 μV/°C of drift over temperature, makes the OPAx388 a great choice for driving high-precision, analog-to-digital converters (ADCs) or buffering the output of high- resolution, digital-to-analog converters (DACs). This design results in excellent performance when driving analog-to-digital converters (ADCs) without degradation of linearity."

     

    There are things that I don't yet understand but that's why I'm doing it - for fun and learning, so I don't mind spending a bit of money to work things out.  I'm trying some things I can do on a breadboard first and then reading around potential solutions for what I'm seeing.  At some point I want to actually produce a PCB because it's as cheap to do that as to get DIL adapters for the ICs!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    ultra-low noise, fast-settling, zero-drift, zero-crossover

    This is where jc2048 advice is welcome, because another player is the current on both OpAmp input sides.

    They have impact on behaviour, and on the resistors you (can) choose to define input impedance and feedback ..

    A lovely subject. It can be analysed without a breadboard, by using a simulator (as suggested by michaelkellett). But if you have the hardware you can see the effects for real too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer