Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Iam using Boost converter LT3958EUHE#PBF..Ia\ need to create time delay around 80ms from input to output..How can I do that?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 317 subscribers
  • Views 435 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Iam using Boost converter LT3958EUHE#PBF..Ia\ need to create time delay around 80ms from input to output..How can I do that?

vandhana
vandhana over 5 years ago

Iam using Boost converter LT3958EUHE#PBF..Ia\ need to create time delay around 80ms from input to output..How can I do that?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 5 years ago +4 suggested
    You aren't really giving us a lot to work with here. I think you mean that you would like the output to turn on 80ms after the input is applied. The good news is that you are using an LT part so experimentation…
  • michaelkellett
    0 michaelkellett over 5 years ago

    You aren't really giving us  a lot to work with here. I think you mean that you would like the output to turn on 80ms after the input is applied.

    The good news is that you are using an LT part so experimentation is free.

     

    Download and install LTSpice (free at www.analog.com).

     

    Run the standard demo for the LT3958.

     

    image

     

    I've added C5 which slows the startup of the chip bet demonstrates it's other problem - there is a path from input to output via L1 and D1.

    This is why the ouput goes to 14V at turn on and then later lifts up to 50V when C5 has charged up a bit.

    There are boosters that don't have this.problem.

     

    Now you tell us a lot more about what you are trying to do (we like schematics and pictures and plenty of words image - and maybe some one can help.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer