Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum coil 100 uH with high quality
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 304 subscribers
  • Views 662 views
  • Users 0 members are here
  • quality
  • high
  • coil
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

coil 100 uH with high quality

Former Member
Former Member over 15 years ago
Hi,
I need a coil 100 uH with high quality ( Q parameter ).
I would like to do LC circuit for frequency 500 kHz. AC and DC current is less than 1 mA.
I have tried different coils and the results were very different. I think that the best was with round toroid.
Is something in the Farnell cataloge what would be appropriate ?
Thanks
Fero
  • Sign in to reply
  • Cancel
Parents
  • nickgray
    0 nickgray over 15 years ago
    You did not say just how small the current through the inductor, just how high you need the Q to be and what is the exact use of the coil. These are very important considerations. The current requirements should include both AC and DC currents. For high frequencies you probably want an inductor with a ferrite core.

    One inductor of 100uH is the JW Miller type 3500-100K, which has a ferrite core, minimum Q of 39 at 796kHz and a saturation current of 800uA. Another 100uH inductor is the JW Miller type 73F-104AF with a ferrite core, minimum Q of 100 at 790kHz a saturation current of 800uA and a 7.7MHz self-resonant frequency.

    For larger currents you might look at the API Delevan S4924-104K with a ferrite core, minimum Q of 50 at 2.5 MHz, saturation current of 113mA and a self-resonant frequency of 10MHz. The JW Miller type 9250-104 has a ferrite core, minimum Q of of 50 at 2.5 MHz, saturation current of 120mA and a self-resonant frequency of 10MHz. The JW Miller type 9250-104-RC has a ferrite core, minimum Q of of 50 at 2.5 MHz, saturation current of 160mA and a self-resonant frequency of 10MHz.

    For information on selecting coils, I suggest looking at http://en.wikipedia.org/wiki/Inductor.

    I hope this information is of some help to you.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • nickgray
    0 nickgray over 15 years ago
    You did not say just how small the current through the inductor, just how high you need the Q to be and what is the exact use of the coil. These are very important considerations. The current requirements should include both AC and DC currents. For high frequencies you probably want an inductor with a ferrite core.

    One inductor of 100uH is the JW Miller type 3500-100K, which has a ferrite core, minimum Q of 39 at 796kHz and a saturation current of 800uA. Another 100uH inductor is the JW Miller type 73F-104AF with a ferrite core, minimum Q of 100 at 790kHz a saturation current of 800uA and a 7.7MHz self-resonant frequency.

    For larger currents you might look at the API Delevan S4924-104K with a ferrite core, minimum Q of 50 at 2.5 MHz, saturation current of 113mA and a self-resonant frequency of 10MHz. The JW Miller type 9250-104 has a ferrite core, minimum Q of of 50 at 2.5 MHz, saturation current of 120mA and a self-resonant frequency of 10MHz. The JW Miller type 9250-104-RC has a ferrite core, minimum Q of of 50 at 2.5 MHz, saturation current of 160mA and a self-resonant frequency of 10MHz.

    For information on selecting coils, I suggest looking at http://en.wikipedia.org/wiki/Inductor.

    I hope this information is of some help to you.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 15 years ago in reply to nickgray
    Hi,
    You're right. I would like to do LC circuit for frequency 500 kHz. AC and DC current is less than 1 mA.
    I have tried different coils and the results were very different. I think that the best was with round toroid.
    Is something in the Farnell cataloge what would be appropriate ?
    Best regards
    Fero Marcincin
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nickgray
    0 nickgray over 15 years ago in reply to Former Member
    The only low current inductor from Farnell that I could find is the TDK MLF2012C101K. It is a surface mount size 0805. It has a Q of 25 at 12 MHz. I could find no 100uH torroid from Farnell and do not know how well this device will work for you.