Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum DC power jack design decision: 2.1mm ID or 2.5mm ID?????
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 340 subscribers
  • Views 38673 views
  • Users 0 members are here
  • jack
  • pcb
  • barrel
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

DC power jack design decision: 2.1mm ID or 2.5mm ID?????

e14 Contributor
e14 Contributor over 16 years ago

Hello there!

We are designing a family of consumer devices that will require an input DC power barrel connector on our PCB.  It will be for +12vdc of various power levels.  We will be able to purchase "off the shelf" UL-listed wall warts depending on the application.  My question is, as I design our PCB to work with a PCB mount DC barrel jack, which is more common?  2.1mm ID or 2.5mm ID for DC power jacks with 5.5mm OD???  So far it looks like they both are "standards".  So, which do I design for if I want to be most forward compatible?  Does one of the options work with both plug types, but not vice-versa?

 

Switchcraft 2.1mm ID, 5.5mm OD $1.61 @ qty=1k

http://search.digikey.com/scripts/DkSearch/dksus.dll?Detail&name=SC1330-ND

 

CUI 2.1mm ID, 5.5mm OD $0.19 @ qty=1k

http://search.digikey.com/scripts/DkSearch/dksus.dll?Detail&name=CP-102A-ND

 

CUI 2.5mm ID, 5.5mm OD $0.19 @ qty=1k

http://search.digikey.com/scripts/DkSearch/dksus.dll?Detail&name=CP-202B-ND

 

Thank you for any suggestions!!.... changing after we make several thousand will be much more difficult!

Respectfully,
Steve  French
814.584.1220.office
814.730.0003.cell
 
President, Volt  Vision
www.voltvision.com
  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 5 years ago in reply to Gough Lui +1
    Yep, more choice in PCB mount but not that many. I wanted a 3-pin, panel mount one that would give me more flexibility in positioning a PCB inside a case and given I already have a 2.1mm 15V wall wart…
  • Gough Lui
    Gough Lui over 5 years ago in reply to Andrew J +1
    I'm sure it will be fine, as long as you're not connecting/disconnecting under load too frequently - the arcs could damage the contacts and increase the contact resistance before the connector reaches…
Parents
  • jemenake
    0 jemenake over 5 years ago

    The 2.1mm-vs-2.5mm dilemma strikes me as kind of a blood type scenario. Where some people can give blood to anybody, others can receive from anybody:

     

    A 2.1mm receptacle:

    • Will be able to have both types of plugs plug into it.
    • Although some 2.5mm plugs have very springy inner contacts (so that they can make a solid contact with a 2.1mm pin), others do not, and, hence, can lose contact if the plug gets wiggled. But, at the very least, if all you have is a 2.5mm plug, you can get your device powered... but you may have to ensure that it doesn't get bumped or moved. Probably the choice when you prefer user-friendliness over solid reliability.

     

    A 2.5mm receptacle:

    • Will not be able to receive a 2.1mm plug. This removes all doubt about which type of connector the user needs. They can only plug in the "correct" size. This could force your user to forestall using your device for a day or two as they shop for the proper power supply.

     

    But your question was about which one was more common/standard. I try to make a habit of trying a 2.1mm plug on every new coaxial-powered device I get, to find out for sure. Lately, it seems like everything I use has a 2.1mm pin on the receptacle.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jemenake
    0 jemenake over 5 years ago

    The 2.1mm-vs-2.5mm dilemma strikes me as kind of a blood type scenario. Where some people can give blood to anybody, others can receive from anybody:

     

    A 2.1mm receptacle:

    • Will be able to have both types of plugs plug into it.
    • Although some 2.5mm plugs have very springy inner contacts (so that they can make a solid contact with a 2.1mm pin), others do not, and, hence, can lose contact if the plug gets wiggled. But, at the very least, if all you have is a 2.5mm plug, you can get your device powered... but you may have to ensure that it doesn't get bumped or moved. Probably the choice when you prefer user-friendliness over solid reliability.

     

    A 2.5mm receptacle:

    • Will not be able to receive a 2.1mm plug. This removes all doubt about which type of connector the user needs. They can only plug in the "correct" size. This could force your user to forestall using your device for a day or two as they shop for the proper power supply.

     

    But your question was about which one was more common/standard. I try to make a habit of trying a 2.1mm plug on every new coaxial-powered device I get, to find out for sure. Lately, it seems like everything I use has a 2.1mm pin on the receptacle.