Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum DC power jack design decision: 2.1mm ID or 2.5mm ID?????
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 340 subscribers
  • Views 38673 views
  • Users 0 members are here
  • jack
  • pcb
  • barrel
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

DC power jack design decision: 2.1mm ID or 2.5mm ID?????

e14 Contributor
e14 Contributor over 16 years ago

Hello there!

We are designing a family of consumer devices that will require an input DC power barrel connector on our PCB.  It will be for +12vdc of various power levels.  We will be able to purchase "off the shelf" UL-listed wall warts depending on the application.  My question is, as I design our PCB to work with a PCB mount DC barrel jack, which is more common?  2.1mm ID or 2.5mm ID for DC power jacks with 5.5mm OD???  So far it looks like they both are "standards".  So, which do I design for if I want to be most forward compatible?  Does one of the options work with both plug types, but not vice-versa?

 

Switchcraft 2.1mm ID, 5.5mm OD $1.61 @ qty=1k

http://search.digikey.com/scripts/DkSearch/dksus.dll?Detail&name=SC1330-ND

 

CUI 2.1mm ID, 5.5mm OD $0.19 @ qty=1k

http://search.digikey.com/scripts/DkSearch/dksus.dll?Detail&name=CP-102A-ND

 

CUI 2.5mm ID, 5.5mm OD $0.19 @ qty=1k

http://search.digikey.com/scripts/DkSearch/dksus.dll?Detail&name=CP-202B-ND

 

Thank you for any suggestions!!.... changing after we make several thousand will be much more difficult!

Respectfully,
Steve  French
814.584.1220.office
814.730.0003.cell
 
President, Volt  Vision
www.voltvision.com
  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 5 years ago in reply to Gough Lui +1
    Yep, more choice in PCB mount but not that many. I wanted a 3-pin, panel mount one that would give me more flexibility in positioning a PCB inside a case and given I already have a 2.1mm 15V wall wart…
  • Gough Lui
    Gough Lui over 5 years ago in reply to Andrew J +1
    I'm sure it will be fine, as long as you're not connecting/disconnecting under load too frequently - the arcs could damage the contacts and increase the contact resistance before the connector reaches…
Parents
  • dougw
    0 dougw over 12 years ago

    Using the smaller pin on the target device allows both sizes of wall wart connector to be used in a pinch. The bigger pin can only be used with the proper mate.

    The bigger pin seems a bit sturdier and should have higher retention force.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 12 years ago

    Using the smaller pin on the target device allows both sizes of wall wart connector to be used in a pinch. The bigger pin can only be used with the proper mate.

    The bigger pin seems a bit sturdier and should have higher retention force.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to dougw

    Be a bit careful with that idea.  I have come across many 2.1mm sockets that don't connect well with the 2.5mm plug.  The 2.1mm pin doesn't always contact the 2.5mm hole properly.  You wouldn't think it possible, but it's bitten me lots of times.

    Here is the solution, a dual 21./2.5 socket:

    http://au.element14.com/webapp/wcs/stores/servlet/Search?catalogId=15001&langId=43&storeId=10184&categoryName=All%20Categories&selectedCategoryId=&gs=true&st=FC681465

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer