Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Low current voltage reference
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 316 subscribers
  • Views 1001 views
  • Users 0 members are here
  • expert
  • reference
  • voltage
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Low current voltage reference

M0DCD
M0DCD over 15 years ago

I have a need to find a suitable device to use as a voltage reference in a low power application. The usual devices (zener diode) seem to need rather more current to get them past the knee into the area where they are actually stable, but the need for say a couple of mA is rather more than I'd want. Looking for anything around 2.5V give or take a few hundred millivolts.

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 15 years ago +1
    Hello, Andrew - I would look at the LT1460-2.5 from Linear Technology. It consumes a maximum of 165uA quiescent current. Other possibilities include the LM4140 , LM4125 and the LM4132 from National Semiconductor…
  • Former Member
    Former Member over 15 years ago +1
    Another one for you to consider... Microchip MCP1525-I/TO 2.5V ref Farnell Order Code: 1292235
  • nickgray
    0 nickgray over 15 years ago

    Hello, Andrew -

     

    I would look at the LT1460-2.5 from Linear Technology. It consumes a maximum of 165uA quiescent current. Other possibilities include the LM4140, LM4125 and the LM4132 from National Semiconductor. the LM4132 is especially interesting with a maximum 100uA quiescent current.

     

    - Nichkolas "Nick" Gray

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 15 years ago

    Another one for you to consider...

     

    Microchip MCP1525-I/TO    2.5V ref 

     

    Farnell Order Code: 1292235

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 15 years ago in reply to Former Member

    Linear tech 1790 http://www.linear.com/pc/productDetail.jsp?navId=H0,C1,C1154,C1002,C1804,P1865

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 15 years ago

    I would recommend using a voltage reference IC. This is the standard technique used for producing a stable accurate reference voltage for Analog-to-Digital Conversion (ADC).

     

    Note that voltage references are not the same as a voltage regulator, in that references tend to only produce a low usable current (less than 100mA), making them largely unsuitable to power a general circuit.

     

    Here are some general links to articles about voltage references:

    • A Quick Guide to Voltage References (Maxim App Note 1182)
    • Voltage References Hold Steady (EDN Paul Rako, 21 Oct 2010)

     

    As you are looking for one with low power / current demands, a 3-terminal Band-gap (series) voltage reference would be a good place to start. Otherwise Floating-Gate-Array (FGA) voltage references such as from Intersil (who acquired Xicon) would also have low quiescent current suitable for battery powered applications.

     

    If you want to know a bit more about topologies and technical differences

    • Understanding voltage references topologies and specifications (Maxim App Note 719)
    • Series of Shunt Reference? (Maxim App Note 4003)

     

    Two short articles written by Texas Instruments' Bonnie Baker in EDN on getting sufficient accuracy from a voltage reference in an ADC circuit (in other words, how to use them correctly).

    • Absorb current spikes and noise with a simple technique (EDN page 22; 21 Oct 2010)
    • Go for the gold with voltage-reference circuits (EDN page 18; 18 Nov 2010)
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 15 years ago

    I think that a voltage reference IC is the best choice. Recently, I used REF3025 from Texas Instruments to produce a 2.5V reference voltage for an ADC converter.

    It features a low quiscient current (50 uA max), a low dropout voltage and a high output current (25 mA).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 15 years ago

    I'm using adjustable references from maxim 61' serie ( if You would need to change voltage ) and LTC6652-2.5 as a reference for ADC.