Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum HELP with uln2003 stepper controller
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 323 subscribers
  • Views 652 views
  • Users 0 members are here
  • uln2003
  • help
  • stepper
  • power
  • motor
  • question
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

HELP with uln2003 stepper controller

Former Member
Former Member over 14 years ago

I am going to be using a uln2003 to as a controller for a stepper motor, interfaced through a computers parallel port, here is a like to the website that I am using for instructions: http://colvins.ca/?p=11  here is a circuit layout:

http://www.instructables.com/files/deriv/FG5/FF7O/FROA0M4W/FG5FF7OFROA0M4W.MEDIUM.jpg

 

This system can be used in place of an expensive stepper controller, the only problem is that the chip will only support up to 500ma, any more then this and the chip blows up.

 

My question is, would it be possible (possibly using ideal diodes) to supply the chip with a low amperage power supply and to supply the motors with a higher amperage using a separate power supply.  Any words of wisdom or ideas would be great!!!

 

Thanks,

Joshua

  • Sign in to reply
  • Cancel

Top Replies

  • Catwell
    Catwell over 14 years ago +2
    Do you need to drive the stepper higher than 0.5A? If so, I would recommend a different setup. However, use the output of the ULN2003 to trigger external power for the stepper coils. ie: Mosfet or power…
  • Catwell
    0 Catwell over 14 years ago

    Do you need to drive the stepper higher than 0.5A? If so, I would recommend a different setup.

     

    However, use the output of the ULN2003 to trigger external power for the stepper coils. ie: Mosfet or power transistor

    Invert logic and connect image

     

     

    Alternatively, you can use a L293DL293D to get 1A

    image

     

    Control lines come from the parallel port of the PC.

     

    Cabe

    http://twitter.com/Cabe_e14
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer