Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum arduino using hall effect sensor and servo
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 305 subscribers
  • Views 801 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

arduino using hall effect sensor and servo

Former Member
Former Member over 13 years ago

I am trying to use a hall effect sensor to activate a servo. I want the servo to move to a specific position when the hall effect sensor is activated and then move back when the sensor is deactivated. When I go to the analog read and look at the values I get from the hall effect sensor, the values are 0 when deactivated, but they range from 195-215 when acivated. I think this is why the servo twitches, but im not certain. I think I should have the input read 0 or 1. When he input is 1 the servo should move to this position and move back for values of 0.  Can you help me out? Heres the code I have so far

 

 

 

 

 

 

#include <Servo.h>

 

Servo myservo;  // create servo object to control a servo

 

int inPin = 0;    // select the input pin for the Hall Effect Sensorr

int val;    // variable to read the value from the analog pin

 

void setup()

{

  myservo.attach(9);  // attaches the servo on pin 9 to the servo object

}

 

void loop()

{

  val = analogRead(inPin);            // reads the value of the Hall Effect Sensorr (value between 0 and 300)

  val = map(val, 0, 300, 0, 20);     // scale it to use it with the servo (value between 0 and 20)

  myservo.write(val);                  // sets the servo position according to the scaled value

  delay(15);                           // waits for the servo to get there

  • Sign in to reply
  • Cancel
Parents
  • billpenner
    0 billpenner over 13 years ago

    look into using a Hall switch. these hall devices are digital. that is they are either on or off. The trigger point is very precise so you can do accurate positioning. Adjustment is simple, just move the magnet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billpenner
    0 billpenner over 13 years ago

    look into using a Hall switch. these hall devices are digital. that is they are either on or off. The trigger point is very precise so you can do accurate positioning. Adjustment is simple, just move the magnet.