Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum arduino using hall effect sensor and servo
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 305 subscribers
  • Views 801 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

arduino using hall effect sensor and servo

Former Member
Former Member over 13 years ago

I am trying to use a hall effect sensor to activate a servo. I want the servo to move to a specific position when the hall effect sensor is activated and then move back when the sensor is deactivated. When I go to the analog read and look at the values I get from the hall effect sensor, the values are 0 when deactivated, but they range from 195-215 when acivated. I think this is why the servo twitches, but im not certain. I think I should have the input read 0 or 1. When he input is 1 the servo should move to this position and move back for values of 0.  Can you help me out? Heres the code I have so far

 

 

 

 

 

 

#include <Servo.h>

 

Servo myservo;  // create servo object to control a servo

 

int inPin = 0;    // select the input pin for the Hall Effect Sensorr

int val;    // variable to read the value from the analog pin

 

void setup()

{

  myservo.attach(9);  // attaches the servo on pin 9 to the servo object

}

 

void loop()

{

  val = analogRead(inPin);            // reads the value of the Hall Effect Sensorr (value between 0 and 300)

  val = map(val, 0, 300, 0, 20);     // scale it to use it with the servo (value between 0 and 20)

  myservo.write(val);                  // sets the servo position according to the scaled value

  delay(15);                           // waits for the servo to get there

  • Sign in to reply
  • Cancel
Parents
  • billabott
    0 billabott over 13 years ago

    Does your servo still twitch?  You may be updating it too quickly.  Add a pause or only send a new value every 10th time throught the loop.

     

    I have some NO reed switches on their way to my house .  The 24 volt 60 watt Rhino Industrial Power Supply arrived today.  The IMO iSmart test and review is going to be in full swing very soon.  On the output side, does anybody really fuse the coil side of a Relay (SPDT 5 Pins 24VDC 10A 120V Contact) to protect the PLC from a short?  Isn't the relay coil much more likely to fail via an open than a short?  Just want to hear some solid professional opinions on that issue.  thanks in advance.

     

    I can certainly understand the need to added safety on the output side of the relay if substantial voltage and/or current is involved.

     

    P.S. I almost forget.  I was reading this awesome discussion of reed and Hall effect device with videos of the test with three different strength Neo-magnets.  It can be found here.  Sorry that it is on a .com site.  Hope that does not offend anyone here.

     

    Cheers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago

    Does your servo still twitch?  You may be updating it too quickly.  Add a pause or only send a new value every 10th time throught the loop.

     

    I have some NO reed switches on their way to my house .  The 24 volt 60 watt Rhino Industrial Power Supply arrived today.  The IMO iSmart test and review is going to be in full swing very soon.  On the output side, does anybody really fuse the coil side of a Relay (SPDT 5 Pins 24VDC 10A 120V Contact) to protect the PLC from a short?  Isn't the relay coil much more likely to fail via an open than a short?  Just want to hear some solid professional opinions on that issue.  thanks in advance.

     

    I can certainly understand the need to added safety on the output side of the relay if substantial voltage and/or current is involved.

     

    P.S. I almost forget.  I was reading this awesome discussion of reed and Hall effect device with videos of the test with three different strength Neo-magnets.  It can be found here.  Sorry that it is on a .com site.  Hope that does not offend anyone here.

     

    Cheers.