Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum DC Voltage / Current Sensor
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 324 subscribers
  • Views 690 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

DC Voltage / Current Sensor

britesc
britesc over 13 years ago

Hi,

 

I need to take continuous voltage and amperage readings from 24 x 2V DC 1200Ah Lead Acid Batteries and pass the information as sensor readings into an Arduino so I can log it and display it on a web page.

 

The batteries voltage and amperage rises up and down during use and charging and quite high during desulphation.

Each bank of 12 batteries rises to 32 Volts (collectively) the amps upto 130 collectively.

 

I am working on a temperature sensor for each battery, but I am also looking for a specific gravity sensor for each battery.

 

I am fairly new to electronics and realise that volatge dividers comes into this somewhere, but I would really love a simple sensor circuit for volatge and another for current if possible.

 

Thank you to anyone who cares to help me. I cannot do onsite checking much anymore as I have become disabled hence neeeding remote checking.

 

Kind regards,

 

jB image

  • Sign in to reply
  • Cancel

Top Replies

  • soumitrab
    soumitrab over 13 years ago +1 suggested
    Hi For voltage checking you can have a voltage divider with 2 resistors in a 1:3 or 1:4 or any other suitable ratio so as to have an acceptable drop within 5v for the comparator/ADC input. Higher value…
  • soumitrab
    0 soumitrab over 13 years ago

    Hi

    For voltage checking you can have a voltage divider with 2 resistors in a 1:3 or 1:4 or any other suitable ratio so as to have an acceptable drop within 5v for the comparator/ADC input. Higher value connects to the +ve rail and you could use the internal or external reference voltage to get actual voltage reading across the divider.

     

    For the current you could use a simple low value (in ohms) but higher wattage resistor for example as a current sensor to read the voltage drop across the sensor via the ADC to get current. Connect the resistor between the battery ground and lead. Alternatively you could also look up current sensors from a host of manufacturers for more accurate readings.

    Hope this helps

    Best wishes

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • soumitrab
    0 soumitrab over 13 years ago in reply to soumitrab

    Just a quick add, ive never used arduino  so please check on the arduino/MCU pinouts/datasheet for the comparators/ADC etc. in case of doubt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • britesc
    0 britesc over 13 years ago in reply to soumitrab

    Thank you very much for your suggestions, I will have a try with my virgin electronics head...

    Kind regards,

     

    jB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • soumitrab
    0 soumitrab over 13 years ago

    Im sure you'll be able to. If you're working on sensors etc with Arduino, this will be a cakewalk for you.

    But just in case, after you setup the resistor divider, calibrate your arduino readings by using the internal reference voltage (or an external 5v reference if youre using a regulated supply) and measuring the voltage from the divider by connecting it to the 5v supply rails. Once you have that reading, you can use the divider for reading higher voltages.

    For the current, use the formula V=IR.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer