Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Improving PFC of series SMPS circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 338 subscribers
  • Views 1017 views
  • Users 0 members are here
  • pfc
  • factor
  • power_
  • series_smps
  • optimizing
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Improving PFC of series SMPS circuit

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

I'm currently having some issues with the Power Factor of an Electronic design (please see attached image: Basic_circuit.png & SMPS_Sch.png) and I was hoping someone could aid me in

optimizing it.

 

Measuring the Power Facter (PF henceforth) on a power meter reveals a PF of only 0.17.

I have tried adding inductance in series with the circuit, but to no avail. PF has decreased if anything.

 

I tried measuring voltage and current from the wall socket to the device using an oscilloscope, to see an indication of the actual PF.

Attached file "LEDS_Volt+Cur_Ph_scope_Cap_2.png" - please be advised: Current measurement is not to scale. Power meter estimated a current of 0.4A.

Voltage and current is definitly out of phase, although a PF of 0.17 seems a bit low.

 

At this point I wanted to try adding active PFC to the circuit, namely a small circuit in the input of the two SMPSes. Unfortunately I

have little to no idea of what kind of circuitry/IC is best used?

Or for that matter whether it will actually do any good in optimizing PF of the system?

 

Do you have some recommendations on designing a small circuit that will improve the Power Factor? Or any advise on generally improving PF?

 

Sincerely yours,

David Larsen

Attachments:
image
image
image
  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 14 years ago

    You can see from your scope traces that a large current is drawn just as the voltage reaches it's peak value - this is normal for a rectifier feeding  a capacitor. Put the inductor BEFORE the capacitor and it will help a bit.

    Try simuating your cicruit (LTSpice is free from www.linear.com).

    Why do you care about the power factor - are you planning to build a lot of these ?

    Is cost an issue ?

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to michaelkellett

    Thank you for your answers.

     

    The application is a LED substitute for flourescent tubes, and hence supposed to fit inside an existing flourescent tube fixture. This means:

     

    1. The input capacitance and inductance cannot be changed. These are mounted in the fixture, and therefore not a part of my actual printboard.

    2. Power factor matters, as these are supposed to replace, say, 100 flourescent tube in industrial (or private) buildings.

    3. Cost is an issue, but only to the extent that implementing an active PFC circuit (i.e. a few dollars worth of components) in the input of the PCB is no problem at all.

     

    I did actually add a ValleyFill circuit to the existing PCB, but it did not improve PF, when measured.

     

    I happen to have read something about harmonics in the current, not present in the voltage, from e.g. switching decrease PF (http://www.cip.ukcentre.com/Power%20Factor.htm).

    Do you know if this is true, and could it be the main reason for the low PF measurement (on Power Meter)?

     

    Thanks once again for your time!

     

    David Larsen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 14 years ago in reply to e14 Contributor

    Hello David,

     

    Certainly you can have harmonics in the current which are not present in the applied voltage. If you are designing  a circuit for mass production you need to invest in some serious test gear - starting with something which can measure harmonics like the

    AIM-TTI INSTRUMENTS - HA1600A

    (one day they'll add a paste as text function to this awful editor)

     

    With a line conditioner this will cost you about £2000 (Farnell sell them).

     

    If your valley fill cicruit didn't help then you got something wrong !

     

    If your plan is to offer  a substitute for a normal fluorescent tube that uses LEDs and goes in a standard fitting  I don't think it's comercially viable - LEDs are only of comparable efficiency with florescents so the pay back time will be very long - BUT - the reflectors etc are designed for a tube which radiates all round and will not be optimum for LEDs so the efficiency of a LED tube in a fluorescent fitting may well be seriously compromised.

     

    I can't really help you more without an answer to the how many - a good design for mass production will use custom silicon. If it's for a special purpose it may not. If you are up to 50W or more into the LEDs you will have to use  a conventional power factor corrected switching supply.

     

    Michael Kellett

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to michaelkellett

    Hello again,

     

    I am terribly sorry about the late reply, but I have been rather preoccupied the last few days.

     

    So what I hear you are saying is: Essentially a Valley-Fill solution should suffice?

    And active PFC might actually be money out the windows?

     

    It is definitely true that actual power saved is not really that much, however, depending on production cost (I am not producing these myself), lifetime of tubes might make such lighting preferable to some people.

    Apparently there is an actual demand for this!

    As an example (in reaction to your post), a single order of 40000 units has just been placed.

     

    Custom silicon is probably not the optimal solution, since the tubes are already in production and basically just need an optimized PFC due to (relatively few) large scale implementations.

     

    With money being tight, though, £2000 equipment is probably out of the question right now, although I do appreciate the need when working more permanently with these types of problems.

    Hopefully, I'll be able to obtain a solution using normal a Power meter!

     

    Thank you once again for your help og advice!

     

    David Larsen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to michaelkellett

    Hello again,

     

    I am terribly sorry about the late reply, but I have been rather preoccupied the last few days.

     

    So what I hear you are saying is: Essentially a Valley-Fill solution should suffice?

    And active PFC might actually be money out the windows?

     

    It is definitely true that actual power saved is not really that much, however, depending on production cost (I am not producing these myself), lifetime of tubes might make such lighting preferable to some people.

    Apparently there is an actual demand for this!

    As an example (in reaction to your post), a single order of 40000 units has just been placed.

     

    Custom silicon is probably not the optimal solution, since the tubes are already in production and basically just need an optimized PFC due to (relatively few) large scale implementations.

     

    With money being tight, though, £2000 equipment is probably out of the question right now, although I do appreciate the need when working more permanently with these types of problems.

    Hopefully, I'll be able to obtain a solution using normal a Power meter!

     

    Thank you once again for your help og advice!

     

    David Larsen