Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum need help picking components
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 304 subscribers
  • Views 395 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

need help picking components

l1t7l3ph0o7
l1t7l3ph0o7 over 13 years ago

Ok I have a project that requires 3 pwm outputs and two digital inputs

I'm looking for an 8-pin MCU where i can just analogWrite to the PWM pins instead of mucking around with software PWM.

 

I've tried the attiny45, but have had no succcess with pwm on three pins, the closest i can get makes one of the inputs high, and i need that input for a button.

Aslo i need to be able to program it with my arduino uno, I see i can program lots of chips with the arduino, so i don't forsee that to be a problem.

 

also using the PWM pins I intend to control three mosfets to control 1 meter 30 led 12v led strip i got from sparkfun.com, and I would like to find a one chip solution to do that, or at least find another way to make the circuit smaller.

 

I am open to using bigger chips, though I need to keep the circuitboard small, it has to fit in a very tight place.

  • Sign in to reply
  • Cancel
Parents
  • nathanjseeley
    0 nathanjseeley over 13 years ago

    The other thing you could use Is some 555 timers for the pwm and then use the attiny45 to handle the button. You can find some 555 calculators on the web so you can get your desired frequency. Infact (from the sound of it) you could almost use 555 timers for the whole project (not that I would recomend that)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nathanjseeley
    0 nathanjseeley over 13 years ago

    The other thing you could use Is some 555 timers for the pwm and then use the attiny45 to handle the button. You can find some 555 calculators on the web so you can get your desired frequency. Infact (from the sound of it) you could almost use 555 timers for the whole project (not that I would recomend that)