Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Electric Trombone: Choosing a suitable slide sensor
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 339 subscribers
  • Views 1950 views
  • Users 0 members are here
  • potentiometer
  • trombone
  • linear
  • slide
  • music
  • sensor
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Electric Trombone: Choosing a suitable slide sensor

e14 Contributor
e14 Contributor over 13 years ago

I've had an idea in my head for a few years now - I'd like to build an electric trombone.

 

This is what I've got in mind:

http://i.imgur.com/YWB22.png

 

The above does look a little ambitious, but perhaps I might get there in the third or fifteenth prototype...

 

 

My main question would be: what is the best sensor to use for the slide?

 

 

The slide has to glide smoothly like a knife through butter, and have as little momentum as possible - so you can do fast passages. The "rod" it moves up and down on should be as light as possible, otherwise there will be quite the moment when both handles are together (a counter balance might be needed...  image).

 

If you hold your left hand to your lips, and position you right hand as far away as possible, then that should be the maximum distance the sensor should have to sense.

 

If the above wasn't limiting enough, then the sensor should also have a good sample rate (in the milliseconds?), and a good sample depth (in the millimeters or fractions of a millimeter?).

 

From time to time, I've looked around for a suitable sensor, but I've never yet found one I've liked.  The closest I've come accross would be to have a softpot with a wiper, or to use graycode on the slde - but I've never really felt satisfied with these solutions.

 

Does anybody know of any sensors that would be suitible for this?

 

Dave

 

Edit:

The MIDI specification for pitch wheels, is to use 16,384 possible variation values over 4 semi tones.  The trombone slide covers 6 semitones (with 7 positions) over aproximately 600mm (about 100mm per semitone).  So to use the same accuracy as a MIDI pitch wheel, the resolution would have to be 16384/4 = 4096 per 100mm, or 40.96 per millimeter.  Obviously, this is a bit of overkill!  I think the best sample deapth would be in the millimeters or fractions of a millimeter.

  • Sign in to reply
  • Cancel
Parents
  • sqkybeaver
    0 sqkybeaver over 13 years ago

    is this going to be attached to a regular trombone? or is this going to be a custom build?

     

    My experiance with the t-bone i think a ultra sonic sensor for the slide would work well. for the mouth piece I'm not sure what you would use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to sqkybeaver

    sheldon bailey wrote:

     

    is this going to be attached to a regular trombone? or is this going to be a custom build?

     

    My experiance with the t-bone i think a ultra sonic sensor for the slide would work well. for the mouth piece I'm not sure what you would use.

    That sounds quite promising.  Take a real trombone mechanism and use a transducer pair to measure the sound delay through the tube.

     

    For a mouthpiece I most heartly recommend the reed and bocal from a bassoon.  Then you have Peter Schickele's tromboon, an instrument required for some of P. D. Q. Bach's works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to sqkybeaver

    sheldon bailey wrote:

     

    is this going to be attached to a regular trombone? or is this going to be a custom build?

     

    My experiance with the t-bone i think a ultra sonic sensor for the slide would work well. for the mouth piece I'm not sure what you would use.

    That sounds quite promising.  Take a real trombone mechanism and use a transducer pair to measure the sound delay through the tube.

     

    For a mouthpiece I most heartly recommend the reed and bocal from a bassoon.  Then you have Peter Schickele's tromboon, an instrument required for some of P. D. Q. Bach's works.