Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum I'm wanting to make a standard sized touchscreen keyboard
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 339 subscribers
  • Views 811 views
  • Users 0 members are here
  • touchscreen_keyboard
  • keyboards
  • touch_screen_controllers
  • touchcreen
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

I'm wanting to make a standard sized touchscreen keyboard

e14 Contributor
e14 Contributor over 13 years ago

I'm looking to make a standard touchscreen keyboard that is fully customizeable.I would like go from the standard qwerty to a gaming "wasd" set up or even shortcuts for programs and switch to mouse capabilities. I have seen some of the touch keyboard that are out there but they seem to be a touch surface with keys set up im thinking more of a tablet style keyboard where it is even a tablet but more the size of a keyboard i would lik to do wireless but wired ok. thanks

 

alex hathaway

  • Sign in to reply
  • Cancel
Parents
  • jds123
    0 jds123 over 13 years ago

    More information would be neccesary help you complete this. Some things that would help are:

    1. Is it touchscreen with a display behind it? Or is it an onscreen keyboard?
    2. How are you looking at using to control it?
    3. When you say custom keys do you mean for launching programs or layouts?
    4. By wireless do you mean bluetooth or WiFi?
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to jds123

    To further explain:

     

    A touch screen with a display behind it.(i.e. much like a touch screen cell phone with a digitizer and an LCD)

     

    I am not sure what or how to control this widget but I think an Android base or even something along the line of the mobile Windows phones and tablets.

     

    A keyboard is normally static the keys are always the keys, but what i am thinking is more of, one million keyboards in one screen. Having available all languages and set ups for any keyboard, also custom keyboards for individual games such as W.O.W. or any other game or drafting program where not all the keys are needed, where you can also set up macros short cuts for the program itself or have a keyboard setup just for kids and learning. all keyboards can be created by one and all and be downloaded as app's from places like Google play or Windows store. this could also be set up for the handicapped large keys or pictures for keys or motion gesture typing for people with less motor skills and even handwriting recognition.

     

    I was thinking more of blue tooth as that gives the keyboard more range but I was also thinking TV remote capabilities like the universal remotes.

     

    Sort of an elongated tablet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to jds123

    To further explain:

     

    A touch screen with a display behind it.(i.e. much like a touch screen cell phone with a digitizer and an LCD)

     

    I am not sure what or how to control this widget but I think an Android base or even something along the line of the mobile Windows phones and tablets.

     

    A keyboard is normally static the keys are always the keys, but what i am thinking is more of, one million keyboards in one screen. Having available all languages and set ups for any keyboard, also custom keyboards for individual games such as W.O.W. or any other game or drafting program where not all the keys are needed, where you can also set up macros short cuts for the program itself or have a keyboard setup just for kids and learning. all keyboards can be created by one and all and be downloaded as app's from places like Google play or Windows store. this could also be set up for the handicapped large keys or pictures for keys or motion gesture typing for people with less motor skills and even handwriting recognition.

     

    I was thinking more of blue tooth as that gives the keyboard more range but I was also thinking TV remote capabilities like the universal remotes.

     

    Sort of an elongated tablet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jds123
    0 jds123 over 13 years ago in reply to e14 Contributor

    A wirless display through bluetooth is a little unrealistic, unless the keymap and icons are not edited often. For the touchscreen I advise researching and finding a touch screen panel and programming it with the arduino, because most touch screens are only four or five wire connections.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to jds123

    So the leg work I've been doing:

     

    custom sized touch screen panel prohibitively expensive

     

    custom sized lcd panel prohibitively expensive

     

    I've started looking into a 17 inch moniter with a resistive overlay to get the same effect

     

    and making it usb/vga attached until I get it working and then go wireless non blue tooth

     

    I have aslo found a keyboard program from Comfort Software "onscreen keyboard"

    (But haven't decided yet)