Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum I'm wanting to make a standard sized touchscreen keyboard
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 339 subscribers
  • Views 812 views
  • Users 0 members are here
  • touchscreen_keyboard
  • keyboards
  • touch_screen_controllers
  • touchcreen
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

I'm wanting to make a standard sized touchscreen keyboard

e14 Contributor
e14 Contributor over 13 years ago

I'm looking to make a standard touchscreen keyboard that is fully customizeable.I would like go from the standard qwerty to a gaming "wasd" set up or even shortcuts for programs and switch to mouse capabilities. I have seen some of the touch keyboard that are out there but they seem to be a touch surface with keys set up im thinking more of a tablet style keyboard where it is even a tablet but more the size of a keyboard i would lik to do wireless but wired ok. thanks

 

alex hathaway

  • Sign in to reply
  • Cancel
Parents
  • phoenixcomm
    0 phoenixcomm over 13 years ago

    Ok This sounds like fun...image

     

    if you had four bars of plastic (from you local hobby shop). now here is the fun part

    you have to drill a series of hole in them along each row. OK? 1 x 1 resolution is probably ok. but you could try .75 or .5

    now you put IR Led's on one side like the top and the bottom.

    now you put IR Detector  on the other side.. OK?

    now mount the rails to the display, make sure that they all line up..

    OK now you can go have a beer.image

     

    So now you have this thing.

    so put a 330 ohm resister and power and ground the resister is to prevent kill your Led's.

    Ok so now they should all be working....  (have another beer image)

    Now the tuff part you have to wire the detector out puts to a CPU pin input.

    you will most likely have to use a I/O expander on the I2C bus.

     

    so when you put your finger into the display your computer input will be high only on two ports one Xn and Yn.

    Do a little math and viola. Now get drunk its done!image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • phoenixcomm
    0 phoenixcomm over 13 years ago

    Ok This sounds like fun...image

     

    if you had four bars of plastic (from you local hobby shop). now here is the fun part

    you have to drill a series of hole in them along each row. OK? 1 x 1 resolution is probably ok. but you could try .75 or .5

    now you put IR Led's on one side like the top and the bottom.

    now you put IR Detector  on the other side.. OK?

    now mount the rails to the display, make sure that they all line up..

    OK now you can go have a beer.image

     

    So now you have this thing.

    so put a 330 ohm resister and power and ground the resister is to prevent kill your Led's.

    Ok so now they should all be working....  (have another beer image)

    Now the tuff part you have to wire the detector out puts to a CPU pin input.

    you will most likely have to use a I/O expander on the I2C bus.

     

    so when you put your finger into the display your computer input will be high only on two ports one Xn and Yn.

    Do a little math and viola. Now get drunk its done!image