Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum I have a few questions for a few people
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 338 subscribers
  • Views 380 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

I have a few questions for a few people

e14 Contributor
e14 Contributor over 13 years ago

I Actually have 2 projects in mind... A small one and a rather large one

 

My first project is a small controller mod to add some buttons on the bottom of my controller to have the default controls more accessable. My 2nd project is an ECU (Engine control circuit). I do know the 2nd project is a bit bigger (like huge) project but im not sure where to start... I was going to go with arduino or similar (Netduino, Maple leaf, etc) and have like a shield for them to do it, but I thought why not do it from scratch.

 

So here is my problems

Project 1:

- Low power (dosent need to be fast)

- 16+ IO ports

- 2 Interrupts

- Vin between 1v8 (or less) to 5v or more (I could regulate it)

 

Project 2:

- Pretty Strong Microcontroller

- Needs to be rather quick (30Mhz + would be nice)

- 35+ IO

- 2+ Interrupts

 

With project 2 (the ECU) I also need to pulse some inductive loads rather quickly (A few milliseconds each) for the injectors and I need to read the Tacho pulse (which is from an inductive load)....

 

I dont need any fancy comunications like CAN or anything, but reading an SD card containg settings would be nice, or maybe an EEPROM or something i dont know...

 

Yes I do know its a big project but I'm sick of making my arduino blink a led and I dont know what else to do with it

 

Some PCB design help would be nice as well (like trace width and length). Even if you cant help, just point me in the direction of somewhere I can read or use to do this project image

 

I will link you to my forum thread at Jaguar Forums so you can get an Idea of what I want to do with the ECU http://www.jaguarforums.com/forum/jaguar-engines-47/custom-jaguar-l-jetronic-5cu-ecu-70295/

 

Thank you for listening to my inquires

  • Sign in to reply
  • Cancel
  • Catwell
    0 Catwell over 13 years ago

    Adin,

     

    Both projects could use a PIC processor. Just pick ones with enough IO.

    Get one of the higher end PICs for project 2, and you are set.

     

    Writing code for a PIC processor is rather easy. If you are not that familiar with programming, try the application "Flowcode." It will let you design visually for the processor you choose.

     

    Keep us all posted on your progress.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer