Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum LIS331DLH accelerometer noise
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 304 subscribers
  • Views 1206 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

LIS331DLH accelerometer noise

jccraig
jccraig over 12 years ago

My board uses a PIC to interface using I2C with an ST accelerometer chip, LIS331DLH. I can read and write to registers okay, at least I can consistently R/W to the control registers for sure. The 8 bytes of X,Y,Z data are extremely noisy though. The low byte in each case is more or less random, the high byte appears to be approximately right, but with some jitter. I've tried different G ranges (2, 4, 8) and different sample rates (50, 100, 400 Hz) and I'm starting to pull my hair out. This is the second prototype board layout, using suggested capacitors etc. All boards act identical. It feels like I'm overlooking some detail in the programming, setup, initialization of the chip, perhaps a detail in my I2C routines, some sort of delay timing issue?  I monitor for data ready in the control register before reading. I'm rather at a loss right now.  Has anyone encountered similar issues with this chip, or can you offer any suggestions for things to check or to be aware of?  Thanks in advance for any help.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    John,

    I am wondering if you have found your noise problem? I am having a similar problem. I don't think that it is noise on my power because I have added caps, removed the debugger, etc. and the problem stays the same.

    I have used this part on a different board and it works fine, so although my code is slightly different, I am setting up the device the same. The design that works is a four layer board, while the broken one is 2. One thing

    I am considering is bad ground on the smt connections on the part. This is a hard thing to test, as there is no access to the under chip pads. Another possibility might be over temp during reflow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    John,

    I am wondering if you have found your noise problem? I am having a similar problem. I don't think that it is noise on my power because I have added caps, removed the debugger, etc. and the problem stays the same.

    I have used this part on a different board and it works fine, so although my code is slightly different, I am setting up the device the same. The design that works is a four layer board, while the broken one is 2. One thing

    I am considering is bad ground on the smt connections on the part. This is a hard thing to test, as there is no access to the under chip pads. Another possibility might be over temp during reflow.