Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum LIS331DLH accelerometer noise
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 304 subscribers
  • Views 1206 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

LIS331DLH accelerometer noise

jccraig
jccraig over 12 years ago

My board uses a PIC to interface using I2C with an ST accelerometer chip, LIS331DLH. I can read and write to registers okay, at least I can consistently R/W to the control registers for sure. The 8 bytes of X,Y,Z data are extremely noisy though. The low byte in each case is more or less random, the high byte appears to be approximately right, but with some jitter. I've tried different G ranges (2, 4, 8) and different sample rates (50, 100, 400 Hz) and I'm starting to pull my hair out. This is the second prototype board layout, using suggested capacitors etc. All boards act identical. It feels like I'm overlooking some detail in the programming, setup, initialization of the chip, perhaps a detail in my I2C routines, some sort of delay timing issue?  I monitor for data ready in the control register before reading. I'm rather at a loss right now.  Has anyone encountered similar issues with this chip, or can you offer any suggestions for things to check or to be aware of?  Thanks in advance for any help.

  • Sign in to reply
  • Cancel
Parents
  • jccraig
    0 jccraig over 12 years ago

    Bruce, it turned out I needed to parse the bits better. I wasn't doing it right, but once I got it working right the "noise" went away.  On a related note, just before we went to our first manufacturing run we learned that ST Micro was replacing the LIS331DLH with a new chip, the LIS3DH.  The footprint is the same, but the internal registers vary some. I didn't have to change my board at all, but I did have to change my program to work with bits that were relocated to some different register locations.  They added some features, and a couple of the pins that weren't used before do have a purpose now, although they can be left tied to either low or high inputs.  The new chip is working well in my first product, which you can see at LucidBrake dot com if you want to check it out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to jccraig

    John

    Very nice product.

     

    Its great to see technology helping to solve problems.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 12 years ago in reply to jccraig

    John

    Very nice product.

     

    Its great to see technology helping to solve problems.

     

    Mark