Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Raspberry Pi + Pico Projector on a Lipo Battery?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 292 subscribers
  • Views 2556 views
  • Users 0 members are here
  • pico_projector
  • raspberry-pi
  • raspberryp-pi
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Raspberry Pi + Pico Projector on a Lipo Battery?

telarium
telarium over 12 years ago

I'm building a project in which I want to power a Raspberry Pi with a small USB hub and a Optoma Pico projector off of a Lipo battery.

 

My battery is a 11.1v 2600 mAh Lipo pack with a 5A 5V switching BEC. The only thing running off the battery is a Raspberry Pi with a USB hub and the projector, which I believe runs off 5v at 1100 mAh.

 

The Pi and the USB hub work, but the projector doesn't. I'm a bit new in power projects, but I was hoping I could get a clue as to why this doesn't seem to work. Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • romain145
    0 romain145 over 12 years ago

    Hi Andrew, I'll try to give you some elements of answer with your problem.

     

    The "Amps" as say Nate isn't the only thing you expect from a power supply. You first expect stability of your output voltage. You can even use a 30A power supply, if you haven't stability you'll just have a *** voltage... image. So I would first check the size of the output capacitor, and add capacitors on that 5V for all the subsequent DC/DC power supplies to have a stable input.

     

    If your Pico Projector isn't charging, that could be due to the instability of the voltage. Another reason can be as simple as the wiring of the cable you're using. I have no idea of the kind of cable provided with your projector, and I assume it's a USB cable.

    I've had some troubles with charging phones from a home made power supply, only because the phone detects it's "own charger" and refuse to charge with any other charger. This is achieved by short-circuiting the 2 data lines of the USB cable inside the charger itself. I just had to do the same wiring and voilà! my phone was charging image.

     

    I'm interested in your project. Keep in mind that LiPo batteries need to be managed, and you MUST use a security interface to switch off if the batteries get low (risk of fire).

    Which Pico Projector are you using ? Is is an HDMI/VGA or a USB projector ?

     

    Good luck ;-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • telarium
    0 telarium over 12 years ago in reply to romain145

    Thanks for the response! I did end up having to use multiple batteries, but I didn't use any capacitors (other than maybe the ones on the SBEC circuits.) All my batteries have protection circuits to hopefully elimate any danger.

     

    The projector I was using was an Optoma PK102. It has HDMI and VGA, but I was using a composite video connection.

     

    I did eventually finish the project and wrote a lengthy blog post about it. If you have the time, check it out! I'd be curious to get your advice on what I could have done differently.

     

    Mini Raspberry Pi Controlled R2D2

    http://www.langleycreations.com/blog/?p=17

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • telarium
    0 telarium over 12 years ago in reply to romain145

    Thanks for the response! I did end up having to use multiple batteries, but I didn't use any capacitors (other than maybe the ones on the SBEC circuits.) All my batteries have protection circuits to hopefully elimate any danger.

     

    The projector I was using was an Optoma PK102. It has HDMI and VGA, but I was using a composite video connection.

     

    I did eventually finish the project and wrote a lengthy blog post about it. If you have the time, check it out! I'd be curious to get your advice on what I could have done differently.

     

    Mini Raspberry Pi Controlled R2D2

    http://www.langleycreations.com/blog/?p=17