Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Cables for IDC connectors  +  Plug for pheonix screw terminals
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 313 subscribers
  • Views 188 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Cables for IDC connectors  +  Plug for pheonix screw terminals

Former Member
Former Member over 12 years ago

I have a NI USB 6343 module circuit board, loaded with 3M - N2534-6002RBN2534-6002RB IDC style male sockets and also the green Pheonix screw terminal blocks. I need to spec a test box and cables that will interface with this USB DAQ.

 

(On the ATE test fixtures I used to work on, the IDC connectors were used inside (Wire wrapped to test pins) and outside (Interfacing with the ATE). I don't recall seeing IDC on actual external cables though.)

 

 

1) For the IDC connectors, do I have to use some kind of ribbon cable to plug into this, or is there a shielded type of cable that I can use to improve noise immunity. I am mostly dealing with e.g. 50uV to 10mV signals.

 

2) For the Pheonix screw terminals, is there a plug that I can use in this, so the operator doesn't have to fiddle wit the screw terminal every time? If so, can I use screened cable with that?

     (NOTE I have in the past seen a plug that can mate with MOLEX - 38630-7806 - TERMINAL BLOCK, 6WAY)

 

3) To connect into the test box, would either euro-fast or military style cylindrical connectors do a good job considering small signal and the requirement for noise immunity?