Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Stepper Motor Behavior
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 336 subscribers
  • Views 663 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Stepper Motor Behavior

e14 Contributor
e14 Contributor over 13 years ago

I have an Arduino Duo interfaced to a Mercury Stepper Motor via an EasyStepper card.

 

My program is simple. It has the motor exercising from 0 steps to 4668 steps, back to 0 and then to -4668 steps. It seems to work fine, except that the motor always seems to do a 2334 step move before starting the move.

 

I am new to the site, and have the sketch for post, but wondered if anyone has any advice.

 

 

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 13 years ago

    Hi Stephen,

     

    I'm not sure I understand the issue 100%. Also, how quickly are you stepping? Any delays in your code?

    You'd probably need to post the code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    Here is the code:

     

    This is an exercise routing to basically move the device back and forth over a 270 degree movement. The stepper motor I am using needs 200 steps for a complete rotation (1.8 degrees per step). Through gear reduction, this amounts to 9336 steps per rotation of the device being stepped.

     

    My goal is to be able to start from a known point, and move the device to preselected locations with input through other arduino pins. It seems to do a +2334 step move before starting the loop. I wrote this exercise routine as a starting point, but am perplexed at this unrequested move from the start.

     

     

    #include <AccelStepper.h>

    // Define a stepper and the pins it will use

     

    AccelStepper stepper(1, 3, 2);

     

    int pos = 7002;

     

    void setup()

    {

     

        stepper.setMaxSpeed(500);

        stepper.setAcceleration(200);

        Serial.begin(9600);

        Serial.println("Ready");

         Serial.println("Currently at ");

         Serial.println(stepper.currentPosition());

     

    }

     

    void loop()

    {

      if (stepper.distanceToGo() == 0)

      

       {

         Serial.println("Currently at ");

         Serial.println(stepper.currentPosition());

         delay(500);

         pos = -pos;

         Serial.println("Moving to ");

         Serial.println(pos);

       }

     

      stepper.runToNewPosition(pos);

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    Hi Stephen,

     

    I'm afraid I can't see what could be the issue. What happens if you comment out all the content in loop()?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    Commenting out the loop was a good suggestion. When gone, nothing at all moved - as expected - but it caused me to rethink and simplify the sketch. I simpled it down and now everthing works as directed by the sketch. I really don't see a lot of difference in the exectuable statements, but it works now. I'll research the cause later.

     

    Thanks for the idea.

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    Commenting out the loop was a good suggestion. When gone, nothing at all moved - as expected - but it caused me to rethink and simplify the sketch. I simpled it down and now everthing works as directed by the sketch. I really don't see a lot of difference in the exectuable statements, but it works now. I'll research the cause later.

     

    Thanks for the idea.

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data