Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum find a suitable NPN transistor part number =?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 303 subscribers
  • Views 462 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

find a suitable NPN transistor part number =?

Former Member
Former Member over 12 years ago

HI expert ,

can you propose a suitable NPN transistor part number =?

My circuit diagram is that this NPN collector terminal is connected to +15V DC power ,then this power will drive a resistor and a LED ,then finally reach to NPN,

so can you propose a suitable NPN part number ?

 

thanks

Choo

image

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 12 years ago

    Hello chow wei,

     

    There are at least two serious problems with your circuit,

     

    The NPN transistor at the top left will be destoyed because you are applying 5V between base and emitter, you need  a resistor in series with the base to limit the current, if you are aiming for say, 20mA in the LED then a good base current would be 1mA so the series resistor should be about 4k7.

     

    The NPN transistors in the bottom row will not share drive as you have drawn them, each one needs its own base resistor - once again 4k7 would be a suitable value.

     

    For the transistors pick and NPN part rated at 30V or more, 100mA minimum

     

    The cheapest suitable types from Farnell are: 2N5551, 2N4401,BC337

     

    The BC337-25, (Farnell 1228215) should be easily available.

     

    As an alternative yoiu could use MOSFETS which don't need the base resistors,  2N7000 would do nicely and are cheap.

     

    There may be other issues with your circuit but I can't tell since you don't say what it is meant to do.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to michaelkellett

    Hi : Michaelkellett

     

     

     

    Base on the below circuit, what type of Part Number  for LED  can be used ?

     

     

     

    Thanks

     

    Chow

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago in reply to michaelkellett

    Hi : Michaelkellett

     

     

     

    Base on the below circuit, what type of Part Number  for LED  can be used ?

     

     

     

    Thanks

     

    Chow