Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum 90 vdc   25 cps Oscilator
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 328 subscribers
  • Views 785 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

90 vdc   25 cps Oscilator

Former Member
Former Member over 12 years ago

I have a Question, 

I want to test my telephone bell for loudness, I understand that the bell rings on   90 VAC 25hz,   or 25 cycles per second.

I would like to buid a simple Full, sign wave Oscelator that will put out 90 VAC  at 25 CPS.  so I can test the bell.

I want it to be solid state.. using house curent, not a battary.

Thank you Richard scott  my email >    r172scott@hotmail.com

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 12 years ago

    To create a 90 VAC 25hz signal for telephone bells can easily be accomplished using a sine wave generator, a 5 Watt audio amplifier and a step up transformer. Because the frequency is lower than the mains frequency,  the transformer needs more turns than a 60 Hz transformer. A transformer designed with a primary winding for 230V and a secondary  winding for 12V could be used to step up the 5Volt 25Hz from the audio amplifier to 90 VAC. For the sine wave generator you can use a standard test instrument or build a wien bridge or RC generator. The volume control of the amplifier can be used to set the output voltage to the desired value. If the frequency of the oscillator is variable, you can change both frequency and amplitude to test the behavior of the telephone bell.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 12 years ago

    To create a 90 VAC 25hz signal for telephone bells can easily be accomplished using a sine wave generator, a 5 Watt audio amplifier and a step up transformer. Because the frequency is lower than the mains frequency,  the transformer needs more turns than a 60 Hz transformer. A transformer designed with a primary winding for 230V and a secondary  winding for 12V could be used to step up the 5Volt 25Hz from the audio amplifier to 90 VAC. For the sine wave generator you can use a standard test instrument or build a wien bridge or RC generator. The volume control of the amplifier can be used to set the output voltage to the desired value. If the frequency of the oscillator is variable, you can change both frequency and amplitude to test the behavior of the telephone bell.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
No Data