Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is this? (RACO 603-3)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 302 subscribers
  • Views 228 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is this? (RACO 603-3)

Former Member
Former Member over 12 years ago

This looks like it may be some kind of potentiometer, or variable resistor. Aluminum casting with two bolt holes, on stepped ears for surface mount. One of the ears has the name(?) RACO embossed in the casting. Two 5mm threaded (electrical) connection posts project from the top. One is isolated (insulated) from the body by non conducting grommet, except for a thin, solid wire wound around the casting (10 wraps/cm, over 6cm, or 60 wraps) and connecting to the opposite post. There is a bridge over the wraps with a thumbscrew locking, adjustable slide that appears to shunt from a variable position on the coil, directly to the opposite pole. The bridge has a slot cut out allong center to accomodate the slide. the top of the cut-out is marked:

N                                                   MAX

     1.22             603-6             12.5

The lower bar is a linear scale from 1 to 10, with the start position, #1 is off-set from the LHS, by approximately slightly wider than the sliding contactor, directly below the first 2 in 1.22. This is a significant component (part) found along side of infrequently used rail-road track.

Attachments: