Hello everyone..i ve just joined element 14..hopefully looking forward to learning a lot from all the users and experts at this forum..anywayz ve been given a project where there is a pulley which is connected to a motor..so as the motor rotates...the pulley functions and does accordingly whatever work it needs to do..the motor is set to 100 revolutions per minute..anyways..however whenever there is load shedding or whenever electricity shuts down.in the plant..the motor needs to start all over again...so through an arduino is there any way...i can tranmit data recording in serial monitor of how much rotations hve taken place..b4 the load shedding occurs..and the 2nd option which is slightly easier iam assuming..is that whenever load shedding occurs..maybe blink an led at the office or smething along dat line..stating dat load sheddign has occurs.i was thinking of RF modules..in this case...as its quite cheap..any suggestions of how can i initiate this project?? Thank You