Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need help connecting Raspberry Pi to old Com-trol MCS-4000 boards.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 3 answers
  • Subscribers 303 subscribers
  • Views 3488 views
  • Users 0 members are here
  • raspberry
  • pi
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need help connecting Raspberry Pi to old Com-trol MCS-4000 boards.

Former Member
Former Member over 12 years ago

Hi All,

 

I have a Raspberry Pi V2 that I'm trying to see if I can connect them to an old Com-trol MCS-4000 control boards.

The Com-trol system had digital & analog input boards and relay output boards. The input and output board use the same IC chip. The IC chip is a p87c51sbpn. It uses UART to communicate.

The Com-trol system is powered with a 24vac transformer. They connect to the boards as (12vac, ct, ground, 12vac).

Then boards are then connected together and to the main console (MCS-4000) via the local bus. The local bus is a serial type communication.

 

How do I check to see if I can connect it to my Pi?

How would I get them to talk to each other?

If I can't us the boards can I just use the p87c51sbpn IC chip.

 

I do have PDF's for the Com-trol system if anyone needs them. They are very hard to find.

 

Teeterbuilt

 

Message was edited by: Teeterbuilt Added PDF's 12/27/13.

Attachments:
imageF_27262_4.pdf
imageF_28077_1.pdf
imageP87C51SBPN datasheet.pdf
  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Hi,

     

    If the communication is based on Rs485, just Google or look at  RS232 to RS485 Converter and Adapter Wiki

    There is a RS 232 port on the Pi (probaly jus 5V or 3.3, check it)

     

    Your have to use an adaptor chip to connect the pi to the RS485 bus.

     

    Do you have the protocol spec ??

     

    greetings Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to Former Member

    Hi Teeterbuilt,

     

    I was little bit short on time.

     

    How do I check to see if I can connect it to my Pi?

         It should but there is some work to do:

              -     The Phi has an RS232 serial bus, your Com-trol system uses an RS485 bus (see your specs)

                   On the RS232 the transmit and receive line are separated, on the RS485 they are combined. But this problem can be overcome

                   -     On the marked are convertor modules available or convertor chips (just what you want, see RS232 to RS485 Converter and Adapter Wiki)

                   -     Just use an convertor or build jour own convertor (its not that complex)

    How would I get them to talk to each other?

                  -         First you have to deal with the hardware (see How do I check to see if I can connect it to my Pi?)

                   -     Then you have to figure out the protocol,( I haven't seen this specs yet, a quick Google search reviled no specs on the protocol)

                   -     For the protocol, try an email comtrol for the protocol specs...

    If I can't us the boards can I just use the p87c51sbpn IC chip.

              -     I think its not useful, the program ROM is a OTP (One time programmable).

     

    I hope this info is of help.

     

    greetings Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to Former Member

    Somehow this discussion seems to be in two places - never mind !

     

    The problem with the RPi RS232 port is that it doesn't actually have one - it has a logic level serial port which can be converted to RS232 (btw RS232 specifies the hardware and signalling voltages and timing of a serial port) by means of an additional chip or board. You could then use one of the readily available RS232-RS485 convertors.

    The big problem is the protocol - if you can't get the supplier (TAC is part of Schneider) to give you documentation you are faced with a big task in reverse engineering it and you would need a complete working system.

    Are you planning on using these boards for a new job or do you have existing installation that you must support ? Is there any reason why you can't just use the original software on a PC ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to michaelkellett

    MK,

         I acquired the full Com-trol system from a remodel job a few years back. I have the main control panel and the input and output boards. I recently had the idea to see of I could use it for model railroading or possibly small home automation. I was just hoping that I could use my RPi to run the input and output board to make them easier to use. The main Com-trol panel is rather difficult to use.

     

    Thanks,

    Teeterbuilt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to michaelkellett

    MK,

         I acquired the full Com-trol system from a remodel job a few years back. I have the main control panel and the input and output boards. I recently had the idea to see of I could use it for model railroading or possibly small home automation. I was just hoping that I could use my RPi to run the input and output board to make them easier to use. The main Com-trol panel is rather difficult to use.

     

    Thanks,

    Teeterbuilt