Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need help connecting Raspberry Pi to old Com-trol MCS-4000 boards.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 3 answers
  • Subscribers 303 subscribers
  • Views 3487 views
  • Users 0 members are here
  • raspberry
  • pi
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need help connecting Raspberry Pi to old Com-trol MCS-4000 boards.

Former Member
Former Member over 12 years ago

Hi All,

 

I have a Raspberry Pi V2 that I'm trying to see if I can connect them to an old Com-trol MCS-4000 control boards.

The Com-trol system had digital & analog input boards and relay output boards. The input and output board use the same IC chip. The IC chip is a p87c51sbpn. It uses UART to communicate.

The Com-trol system is powered with a 24vac transformer. They connect to the boards as (12vac, ct, ground, 12vac).

Then boards are then connected together and to the main console (MCS-4000) via the local bus. The local bus is a serial type communication.

 

How do I check to see if I can connect it to my Pi?

How would I get them to talk to each other?

If I can't us the boards can I just use the p87c51sbpn IC chip.

 

I do have PDF's for the Com-trol system if anyone needs them. They are very hard to find.

 

Teeterbuilt

 

Message was edited by: Teeterbuilt Added PDF's 12/27/13.

Attachments:
imageF_27262_4.pdf
imageF_28077_1.pdf
imageP87C51SBPN datasheet.pdf
  • Sign in to reply
  • Cancel
Parents
  • robotop
    0 robotop over 11 years ago

    Hello, looking at the PDF you supplied, the communications acts via RS485 interface, with baud rate of 19200 or 38400 BPS. You can simply use an USB to RS485 interface that can be recognized by the Raspberry PI board, then use it in your program as TTYUSB0 (or similar), setting the appropriate baud, bits and parity parameters. Note that if you use an FTDI based interface, the handling of the bus direction (RS485 is always half-duplex) is done directly by the interface, so you have just to write to the serial channel or read from it, without the need for the direction control (usually involving one output line as TX enable). The FTDI chips have an automatic "1 bit before start" activation of transmission and "1 bit after stop bit" release of the bus. So, when you don't transmit any data, the receiver is enabled, and when you transmit data, the transmitter is enabled just for the requested time, freeing the bus immediatly after the data has been transmitted. Obviously, the hardware part is very simple, but you must know the protocol for sending and retrieving data. Note that the RS485 bus is multi-point, so every device connected has its own "address". I noted on the schematic that there are two rotary switches to set the address for the peripheral. However, if you don't have the protocol specs (a list of commands and the packet structure) it's almost impossible to handle it. It may be "easily" decoded if you have some controller that actually works with the device. In such case, you can use the USB to RS485 interface as a "sniffer" on the bus, capturing the packets that go from the controller to the device and vice-versa. Hope this helps...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to robotop

    Emilio,

         I am in the process of looking for a rs485 adapter. Since I do not have documentation on the protocols I was planning to use the rs485 as a sniffer. Thank for describing how the rs485 works. Yes there is one address rotary knob on the board 0-F.

     

    Thanks,

    Teeterbuilt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Just popping up:

     

    When your sniffing the protocol, just check the MODBUS protocol. Its widely used and plain ASCII, documents are easily found on the internet.

     

    good luck !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Just popping up:

     

    When your sniffing the protocol, just check the MODBUS protocol. Its widely used and plain ASCII, documents are easily found on the internet.

     

    good luck !