Hi All,
I have a Raspberry Pi V2 that I'm trying to see if I can connect them to an old Com-trol MCS-4000 control boards.
The Com-trol system had digital & analog input boards and relay output boards. The input and output board use the same IC chip. The IC chip is a p87c51sbpn. It uses UART to communicate.
The Com-trol system is powered with a 24vac transformer. They connect to the boards as (12vac, ct, ground, 12vac).
Then boards are then connected together and to the main console (MCS-4000) via the local bus. The local bus is a serial type communication.
How do I check to see if I can connect it to my Pi?
How would I get them to talk to each other?
If I can't us the boards can I just use the p87c51sbpn IC chip.
I do have PDF's for the Com-trol system if anyone needs them. They are very hard to find.
Teeterbuilt
Message was edited by: Teeterbuilt Added PDF's 12/27/13.