Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Very low friction potentiometer or encoder
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 342 subscribers
  • Views 3920 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Very low friction potentiometer or encoder

tobbera
tobbera over 12 years ago

Hi!

 

Hope you can help me. I'm going to build a wind vane that senses wind direction. For this I need a rotary position sensor such as a potentiometer or encoder. Its going to be connected to and Arduino Uno

 

                  *360 degrees rotation without stop.

    • *Very low friction (free spinning)
    • *Resolution of at least 360 per revolution.
    • *Dead band of  up to 45 degrees is OK
    • *Ruggedness and durability is not of great concern, this is for an experiment.
    • *Bellow USD $50

 

I have looked at several online, but found many to be very expensive. I have bought a BOURNS 6639S-1-103, but it simply has too much friction

  • Sign in to reply
  • Cancel
Parents
  • sirmorris
    0 sirmorris over 12 years ago

    You could attach a tiny strong magnet to the vane. Arrange a halo of hall effect sensors on the shaft nearby. They're really easy to use, and cheap. If you're pin limited you could multiplex them in groups, otherwise you just need to read which of the detectors is registering a magnet nearby. If you're only after 45 degree resolution you could probably get away with 8. You should select a sensor type which can detect over a relatively wide area, the orientation of some needs to be tightly controlled. This should avoid dead space between the sensors. I see that you don't want to build an enclosure around the detector but you could probably construct this 'dead bug' style in a little over the same volume you would be allocating to a pot.

     

    Charlie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sirmorris
    0 sirmorris over 12 years ago

    You could attach a tiny strong magnet to the vane. Arrange a halo of hall effect sensors on the shaft nearby. They're really easy to use, and cheap. If you're pin limited you could multiplex them in groups, otherwise you just need to read which of the detectors is registering a magnet nearby. If you're only after 45 degree resolution you could probably get away with 8. You should select a sensor type which can detect over a relatively wide area, the orientation of some needs to be tightly controlled. This should avoid dead space between the sensors. I see that you don't want to build an enclosure around the detector but you could probably construct this 'dead bug' style in a little over the same volume you would be allocating to a pot.

     

    Charlie