Hello world. I'm new here and I would like to start learning about electronics. It's something that fascinates me, but I know close to nothing about it.
Last week I installed an alarm on my car by myself and I got it to work perfectly.
Now, what I'd like to do is to install a cellphone in the car, take the signal from the lights that flash when the alarm is triggered and use it to dial my phone number by using the speed dial function on the phone that will be in the car.
So far I have the following:
- firstly, the signal from the alarm is a 12V DC current that is intermintent. It is on 1 second and off 1 second. There, I figured I could use a reservoir capacitor in order to have a (almost) constant signal.
- that signal would operate a relay that will make a connection between the two contacts on a number key in the cellphone, so that after 3 or 4 seconds, the speed dial would call my number.
(* I could use a separate relay that uses the wires that feed a relay to disconnect the energy from the spark plugs when the alarm is triggered, to avoid the phone calling when I connect or disconnect the alarm, since lights flash in that moment.)
- What I'd need is that the relay that closes the circuit on the phone (i.e. dial the number through speeddial) work for no more than 5 seconds (about the time it takes for the speed dial to activate)
- After that, I'd like for the circuit to wait for about 1 or 2 minutes and start over (so as to no call me again as soon as I hang up) to remind me after 1 or 2 minutes that the alarm is still ringing if I didn't catch it the first time.
I've attached a very crude diagram (the only imaging SW I know how to use is AutoCAD, but I don't have it installed, so I used Paint) of how I think it might work. But that will only keep the cellphone button pressed for as long as the alarm is ringing.
All of this should be while the alarm is triggered, which is to say that the intermitent pulse from the lights flashed by the alarm should be ignored for 1 or 2 minutes.
I've read something about a 555 IC that would be usefull to get the timing (the 5 sec on and 1 minute off) but i hace no idea how to use it and where to put it.
The end result would be:
the car alarm is triggered and the car lights will flash (one second on, one second off) continuosly. Once the lights start flashing, helped by the capacitor (and enabled by the second relay, which only activates when the alarm is triggered and not when the alarm is armed or disarmed) the main relay will hold a number key in the phone's keypad, which will make it call me using the speed dial feature in the car's phone.
After that, the relay will disconnect (the key in the phone will no longer be pressed); it will wait a minute and call me again (as long as the alarm is still active).
Would you be so kind to help me?
I'm very excited about this project. It should seem very simple and basic to the members of the community, but it would be HUGE for me and it would encourage me to undertake more ambitous projects and to learn more about electronics.
Thanks!!!
P.S.: Since I'm new here, I'm not sure if this thread goes in this forum. If not, could you be so kind to move it where it should go? or at least tell me where I should post it.
P.S.2: Ben Heck rules!!!