Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum welder current adjustment and measurement
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 309 subscribers
  • Views 4056 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

welder current adjustment and measurement

Former Member
Former Member over 11 years ago

Hello everyone, over the past few months I have been interested in building ARC welders from microwave transformers, after my prototype version I decided to add more features to my second model one of which would be adjusting and displaying current output. The problems I have been facing are developing an accurate  way to vary the amps and to locate a high amp digital meter. If any of you have any methods for varying current and or know a device that can measure high current your help would be greatly appreciated.Thank you

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 11 years ago

    The best way to control the amps of your secondary is to control the voltage of your primary. For this you could use a triac or even a commercial light dimmer control of sufficient current handling capacity. I do not know how many amps you are talking about and I do not know what your circuit looks like but since you are talking transformers I will assume you are trying to measure AC amps. You can make your own ampmeter by winding a coil around one of the transformer secondary wires and using the induced voltage to drive a milli or micro volt meter with a shunt resistor. Set up a resistive load on your secondary so you have a known current, say 10 amps, flowing. Add or subtract winds of the coil around the wire until your meter reads 10 accross the shunt resistor. Then you will have a correspondence between the Amps of your secondary and the millivolts of your meter. As I am fairly old school I will not be the least bit surprised to find out there is a better way to do this but this should get the discussion going.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to jw0752

    Hi Hampton,

    Check out and take the information from Don seriously. He is very smart and intuitive. Sometimes I don't understand his advice right away but it is usually very good. I had another idea for the control of the current. You could use a Variac. I do not know where you are located but almost every older Dental X-Ray machine has a variac built in for controlling the Kvp of the x-ray. If you went to a dental supply house they may have an old x-ray unit you could salvage. The variac will allow you to control the voltage to the primary of your transformer and even boost it. I know they are capable of 15 amps at 120 VAC for short time periods. I am not sure what they can handle continuous duty. The x-ray will draw upwards of 15 amps but then for only 1/2 second. My other idea with the light dimmer would not control the voltage but rather the duty cycle of the power to the primary. I don't understand your application well enough to know which would be better. In my area the dimmer controls are available from hardware stores or electrical equipment suppliers. Don's Idea for using a precision .01 ohm resistor in your secondary would allow you to use a digital volt meter to read the voltage drop across it.  For example if you measured 3 volts across a .01 ohm resistor you would know that there was 300 amps flowing. If you don't need the precision of of a commercial resistor you could build your own by looking at the specs on wire gauge, length and resistance and make your own .01 ohm resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to jw0752

    Hi Hampton,

    Check out and take the information from Don seriously. He is very smart and intuitive. Sometimes I don't understand his advice right away but it is usually very good. I had another idea for the control of the current. You could use a Variac. I do not know where you are located but almost every older Dental X-Ray machine has a variac built in for controlling the Kvp of the x-ray. If you went to a dental supply house they may have an old x-ray unit you could salvage. The variac will allow you to control the voltage to the primary of your transformer and even boost it. I know they are capable of 15 amps at 120 VAC for short time periods. I am not sure what they can handle continuous duty. The x-ray will draw upwards of 15 amps but then for only 1/2 second. My other idea with the light dimmer would not control the voltage but rather the duty cycle of the power to the primary. I don't understand your application well enough to know which would be better. In my area the dimmer controls are available from hardware stores or electrical equipment suppliers. Don's Idea for using a precision .01 ohm resistor in your secondary would allow you to use a digital volt meter to read the voltage drop across it.  For example if you measured 3 volts across a .01 ohm resistor you would know that there was 300 amps flowing. If you don't need the precision of of a commercial resistor you could build your own by looking at the specs on wire gauge, length and resistance and make your own .01 ohm resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to jw0752

    Hello Mr. Wiltrout, I like your variac idea but I doubt I would have the funds or the access to the machine due to the fact that I am only fourteen. I will try the resistor method for measuring the current from the secondary, but I was wondering whether the resistor is meant to be in parallel or series with the output I assume parallel because Mr. Hersey said to measure the drop across the resistor. And I believe I understand the relationship between the voltage and the amps in that method based on Ohm's law the volts relate directly to the amps so measuring the volts will allow you to calculate the amps. Also would it work to use a 1 ohm resistor instead of a .01 ohm so the volt meter would display the exact current? Thank you for your explanation of the volt meter method.:)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Thank you also Mr. Hersey for your idea I believe I will use it in my project.:)