Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum welder current adjustment and measurement
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 306 subscribers
  • Views 4006 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

welder current adjustment and measurement

Former Member
Former Member over 11 years ago

Hello everyone, over the past few months I have been interested in building ARC welders from microwave transformers, after my prototype version I decided to add more features to my second model one of which would be adjusting and displaying current output. The problems I have been facing are developing an accurate  way to vary the amps and to locate a high amp digital meter. If any of you have any methods for varying current and or know a device that can measure high current your help would be greatly appreciated.Thank you

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 11 years ago


    Hi Hampton,

    The resistor that Don was talking about would be put in SERIES with your load. If this is a welder it would be in series with the Arc. If you put it across the secondary voltage it would short it out.  You have to keep the resistance very small when you are working with large currents or the test resistor will have to dissipate too much power. At the 300 amps you mentioned a 1 ohm ohm resistor would have to dissipate 90,000 watts. We are obviously in fantasy land here. Good luck on your project and be very careful of the danger from high voltages. It may be better to work on some low voltage projects.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago


    Hi Hampton,

    The resistor that Don was talking about would be put in SERIES with your load. If this is a welder it would be in series with the Arc. If you put it across the secondary voltage it would short it out.  You have to keep the resistance very small when you are working with large currents or the test resistor will have to dissipate too much power. At the 300 amps you mentioned a 1 ohm ohm resistor would have to dissipate 90,000 watts. We are obviously in fantasy land here. Good luck on your project and be very careful of the danger from high voltages. It may be better to work on some low voltage projects.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 11 years ago in reply to jw0752

    Guys

    Conventional Arc welders usually use about 50-60v to strike and then a lot lower to maintain the arc.

    The newer inverter welders are often higher at 90v strike, which makes them much easier to use.

     

    In a conventional welder the air gap limits the current available to the stick, (so its basically an transformer with adjustable efficiency).

    IMO you would be much better trying to control the input side of the welder, than the load side.

     

    I've always found the current to be a guideline, as the arc eventually dictates the current and weld quality obtained.

    Bear in mind that you still need to maintain a certain voltage to keep the arc, and this also depends on the type of rod you use.

     

     

    I would have thought that conventional welders were so cheap. Here in NZ you can pickup a lower quality brand new for $NZ160 or second hand for $50-60

    Inverter welders are probably more worth the effort due to their higher cost, however these have relatively expensive parts that can go bang quite easily.

     

    Also with a single phase welder, you would be lucky to get much more than 150-160A as it would overrate the mains supply.

    For a 300A welder, you're either talking about a very low duty cycle (ie weld time v cooling time) or a serious piece of kit.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to jw0752

    That makes sense why a higher ohm resistor would overheat,, though would a higher watt resistor have better temperature compensation? Also in my earlier comment I mistakenly said I thought the resistor was supposed to be in parallel but I understand why it should be in series.

    Thank you