Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum DRV102!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 2 answers
  • Subscribers 316 subscribers
  • Views 2564 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

DRV102!

Former Member
Former Member over 11 years ago

regarding the duty cycle of TO220 How to adjust the duty cycle continuously for example from 20% to 50% to 90% and so on at one operation?

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi,  The designation TO 220 is a case style of a transistor, SCR, or Triac. If properly heat sunk and not over driven the TO-220 case is easily capable of 100% duty cycle. You will have to give us more information on your circuit and application for more information.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to jw0752

    first of all thanks for reply

    actually i want to derive a solenoid valve to control the flow of air pressure .This air  pressure is connected to a cylinder which in turn used to pull up the suspension car model but controlled by the previous solenoid valve.so i want  by using the DRV102(TO220) to derive the solenoid valve and by adjusting the duty cycle which is allowable in DRV102 to see the the different height of the suspension car model increase or decrease proportional to duty cycle for example from %20 to %30 to %50 and so on.......

    http://www.ti.com/lit/ds/sbvs009b/sbvs009b.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to jw0752

    first of all thanks for reply

    actually i want to derive a solenoid valve to control the flow of air pressure .This air  pressure is connected to a cylinder which in turn used to pull up the suspension car model but controlled by the previous solenoid valve.so i want  by using the DRV102(TO220) to derive the solenoid valve and by adjusting the duty cycle which is allowable in DRV102 to see the the different height of the suspension car model increase or decrease proportional to duty cycle for example from %20 to %30 to %50 and so on.......

    http://www.ti.com/lit/ds/sbvs009b/sbvs009b.pdf