Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum DRV102!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 2 answers
  • Subscribers 316 subscribers
  • Views 2554 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

DRV102!

Former Member
Former Member over 11 years ago

regarding the duty cycle of TO220 How to adjust the duty cycle continuously for example from 20% to 50% to 90% and so on at one operation?

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    This is a neat chip!  IDK how suited it is for uP control, though.  It seems like the thing to do would be to use the PWM on the uP to generate the (control voltage) CV.  Which seems a little Rube Goldberg.  For some reason many uP manufacturers include A/D but often leave us with some rather crude PWMs for analog out.  For a uP that had on-board D/A, this would be one nifty ticket!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    This is a neat chip!  IDK how suited it is for uP control, though.  It seems like the thing to do would be to use the PWM on the uP to generate the (control voltage) CV.  Which seems a little Rube Goldberg.  For some reason many uP manufacturers include A/D but often leave us with some rather crude PWMs for analog out.  For a uP that had on-board D/A, this would be one nifty ticket!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to D_Hersey

    thanks a lot

    which uP board u think it has an analog output??